4.1 Internal Preprocessor
The assembler has an internal preprocessor. The internal processor performs the following actions.
- Adjusts and removes extra white space. It leaves one space or tab before the keywords on a line, and turns any other white space on the line into a single space.
- Removes all comments, replacing them with a single space, or an appropriate number of new lines.
- Converts character constants into the appropriate numeric value.
The internal processor does not perform the following actions.
- macro preprocessing
- include file handling
- anything else you may get from your C compiler’s preprocessor
You can do include file preprocessing with the .include directive. See Assembler Directives.
You can use the C compiler driver to perform other C-style preprocessing
by ensuring the input file uses a .S extension. For
additional information on the compilation driver, see the compiler user's guide relevant
for your target device.
If the first line of an input file is #NO_APP or if you use the -f option, white space and comments are not removed from the input file. Within an input file, you can ask for white space and comment removal in certain portions by putting a line that says #APP before the text that may contain white space or comments, and putting a line that says #NO_APP after this text. This feature is mainly intended to support assembly statements in compilers whose output is otherwise free of comments and white space.