11.2 Locating Objects at a Specific Address
In this example, the C language array
buf1 is located at an absolute address in data memory. The address of buf1 can be confirmed by executing the program in the
simulator, or by examining the link
map.#include <stdio.h>
int __attribute__((address(0xa0000200))) buf1[128];The equivalent array definition in assembly language appears below. The
.align directive is optional and represents the
default alignment in data memory. Use of * as a section
name causes the assembler to generate a unique name based on the source file
name. .globl buf1
.section .bss.buf1, address(0xa0000200), bss
.align 2
.type buf1, @object
.size buf1, 512
buf1:
.space 512Note that if another object is manually allocated to a section used for an absolute object
(for example, using the section attribute), then only one of those objects
will be found at the specified section link address. Consider a structure if there are
multiple objects to be positioned and their order is important.