8.3.1 Start-group/End-group Options
The --start-group archives,
--end-group option marks the start and end of a group of library archives.
The archives argument should be a list
of library archive files (.a extension) or -l options. The specified archives are searched repeatedly until no new
undefined references are created. Normally, an archive is searched only once in the order
that it is specified on the command line. If a symbol in that archive is needed to resolve
an undefined symbol referred to by an object in an archive that appears later on the
command line, the linker would not be able to resolve that reference. By grouping the
archives, they will all be searched repeatedly until all possible references are resolved.
Using this option can negatively impact performance, so it is best to use it only when
there are unavoidable circular references between two or more archives.