9.5.5.6 Output Section Address
The address is an expression for the VMA
(the virtual memory address) of the output section. If address is not provided, the linker
will set it based on region if present, or otherwise based on the current value of the
location counter.
If address is provided, the address of
the output section will be set to precisely that. If neither
address nor
region is provided, then the address of the output
section will be set to the current value of the location counter aligned to the alignment
requirements of the output section. The alignment requirement of the output section is the
strictest alignment of any input section contained within the output section.
.text . : { *(.text) }and.text : { *(.text) }are
subtly different. The first will set the address of the .text output section to the current value of the location counter. The second
will set it to the current value of the location counter aligned to the strictest alignment
of a .text input section.0x10 byte boundary, so that the lowest
four bits of the section address are zero, the command could look like
this:.text ALIGN(0x10) : { *(.text) }The above command works because ALIGN
returns the current location counter aligned upward to the specified value.
Specifying address for
a section will change the value of the location counter.