8.6.8 Warn-common Option
The
--warn-common option warns when a
common symbol is combined with another common symbol or with a symbol definition.
This option allows you to find potential problems from combining global symbols.
There are three kinds of global symbols, illustrated here by C
examples:int i = 1;A definition, which goes in the initialized data section of the output
file.
extern int i;An undefined reference, which does not allocate space. There must be
either a definition or a common symbol for the variable
somewhere.
int i;A common symbol. If there are only (one or more) common symbols for a variable, it goes in the uninitialized data area of the output file.
The linker merges multiple common symbols for the same variable into a single symbol. If they are of different sizes, it picks the largest size. The linker turns a common symbol into a declaration, if there is a definition of the same variable.
The --warn-common option can produce five kinds of warnings. Each warning consists of a pair of lines: the first describes the symbol just encountered, and the second describes the previous symbol encountered with the same name. One or both of the two symbols will be a common symbol.
Turning a common symbol into a reference, because there is already a
definition for the
symbol.
file(section): warning: common of ‘symbol’ overridden by definition
file(section): warning: defined hereTurning a common symbol into a reference, because a later definition for
the symbol is encountered. This is the same as the previous case, except that the
symbols are encountered in a different
order.
file(section): warning: definition of ‘symbol’ overriding common
file(section): warning: common is hereMerging a common symbol with a previous same-sized common
symbol.
file(section): warning: multiple common of ‘symbol’
file(section): warning: previous common is hereMerging a common symbol with a previous larger common
symbol.
file(section): warning: common of ‘symbol’ overridden by larger common
file(section): warning: larger common is hereMerging a common symbol with a previous smaller common symbol. This is the
same as the previous case, except that the symbols are encountered in a different
order.
file(section): warning: common of ‘symbol’ overriding smaller common
file(section): warning: smaller common is here