35.5 ADC Parameter Definitions
An ideal n-bit single-ended ADC converts a voltage linearly between GND and
            VREF in 2n steps (LSb). The lowest code is read as
            ‘
   0’, and the highest code is read as ‘2n-1’. Several
         parameters describe the deviation from the ideal behavior:- Offset Error
 - The deviation of the first transition (0x000 to 0x001) compared to
                  the ideal transition (at 0.5 LSb). Ideal value: 0 LSb. 
Figure 35-1. Offset Error  - Gain Error
 - After adjusting for offset, the gain error is found as the deviation
                  of the last transition (e.g., 0x3FE to 0x3FF for a 10-bit ADC) compared to the
                  ideal transition (at 1.5 LSb below maximum). Ideal value: 0 LSb.
Figure 35-2. Gain Error  - Integral Nonlinearity (INL)
 - After adjusting for offset and gain error, the INL is the maximum
                  deviation of an actual transition compared to an ideal transition for any code.
                  Ideal value: 0 LSb.
Figure 35-3. Integral Nonlinearity  - Differential Nonlinearity (DNL)
 - The maximum deviation of the actual code width (the interval between
                  two adjacent transitions) from the ideal code width (1 LSb). Ideal value: 0
                     LSb.
Figure 35-4. Differential Nonlinearity  - Quantization Error
 - Due to the quantization of the input voltage into a finite number of codes, a range of input voltages (1 LSb wide) will code to the same value. Always ±0.5 LSb.
 - Absolute Accuracy
 - The maximum deviation of an actual (unadjusted) transition compared to an ideal transition for any code. This is the compound effect of all errors mentioned before. Ideal value: ±0.5 LSb.