3.3.2 Smart Appliance Control on PIC32CM JH01 Curiosity Nano+ Touch Evaluation Kit

Download

Description

This application demonstrates a smart fan control system that operates in two distinct modes:
  • Temperature Control mode
  • BLE Control mode
Users can switch between these modes using the touch sensor built into the Curiosity Nano board. Upon initialization, the application defaults to Temperature Control mode. A single press on the touch sensor activates BLE Control mode, while a subsequent press reverts the system to Temperature Control mode. In addition, once the device is in BLE Control mode, users can revert to Temperature Control mode by either employing the touch sensor or issuing a BLE command.
  1. Temperature Control mode: Automatically controls the DC fan based on the temperature measurement from Weather Click. Both the temperature value and fan speed are displayed on e-paper display. The temperature ranges for the respective fan speed are:
    1. Temperature between 18 (64 F) to 25 (77 F) degree Celsius, the fan rotates at LOW speed.
    2. Temperature between 26 (78 F) to 30 (86 F) degree Celsius, the fan rotates at MEDIUM speed.
    3. Temperature is greater than 30 degree Celsius (86 F), the fan rotates at HIGH speed.
    4. Temperature is less than 18 (64 F), the fan is switched OFF.
  2. BLE Control mode: Control the DC fan based on BLE commands from Microchip Bluetooth Data (MBD) app in smartphone. Besides, the user will be able to switch back to Temperature Control mode. The available commands for use are:
    1. FAN_ON: Turns ON the fan at LOW speed.
    2. FAN_OFF: Turns OFF the fan.
    3. FAN_LOW: Runs the fan at LOW speed.
    4. FAN_MID: Runs the fan at MEDIUM speed.
    5. FAN_HIGH: Runs the fan at HIGH speed.
    6. TEMP_MODE: Switches to Temperature Control mode.

Modules/Technology Used

  • Peripheral Modules

    • SYSTICK
    • Timer
    • SERCOM (I2C)
    • SERCOM (USART)
    • SERCOM (SPI)
    • PTC
    • RTC
    • Wireless RNBD Driver
    • STDIO library
    • Touch library
    The following figure provides the MCC Harmony project graph with all the components.

Hardware Used

Software/Tools Used

This project has been verified to work with the following versions of software tools:

Refer to the Project Manifest present in harmony-manifest-success.yml under the project folder pic32cm_jh01_cnano_smart_appliance_control/firmware/src/config/pic32cm_jh01_cnano.

Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version.

Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, it is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).

Hardware Setup

  • Mount PIC32CM JH01 Curiosity Nano evaluation kit on CNANO56_HOST_CONN (U3) connector of Curiosity Nano Base board
  • First connect the 4 wires from the Fan Click to the Fan (Red wire to +5V, Black wire to GND, Blue wire to PWM and Yellow wire to TACH of the Fan Click) and then mount the Fan Click board onto mikroBUS socket 1 connector of Curiosity Nano Base. The fan click uses the SERCOM0 I2C interface
  • Mount the Weather Click board onto mikroBUS socket 2 connector of Curiosity Nano Base. This Weather Click uses the SERCOM0 I2C interface
  • Connect the RNBD451 Add On Board to the mikroBUS socket 3 connector of Curiosity Nano Base. The RNBD module uses the SERCOM4 USART interface
  • Connect the mikroBUS Xplained Pro to EXT 1 connector of Curiosity Nano Base board and mount the eINK Click and e-paper display onto the mikroBUS Xplained Pro. The e-paper display uses the SERCOM2 SPI interface
  • Connect the Lipo Battery to J1 connector of PIC32CM JH01 Curiosity Nano evaluation kit and make sure battery switch is toggled to Battery ON position
  • Connect the PIC32CM JH01 Curiosity Nano evaluation kit to the host PC as a USB device, through a Type-A male to micro-B USB cable connected to Micro-B USB (Debug USB) port

Programming Hex File

The pre-built hex file can be programmed by following the below steps.

Steps to program the hex file
  • Open MPLAB X IDE
  • Close all existing projects in IDE, if any project is opened
  • Go to File>Import>Hex/ELF File
  • In the Import Image File window,
    1. Create Prebuilt Project,
      • Click the Browse button to select the prebuilt hex file
      • Select Device as PIC32CM5164JH01048
      • Ensure the proper tool is selected under Hardware Tool and click the Next button
    2. Select Project Name and Folder,
      • Select appropriate project name and folder and click the Finish button
  • In MPLAB X IDE, click the Make and Program Device button to program the device
  • Follow the steps in Running the Demo section

Programming/Debugging Application Project

  • Open the project pic32cm_jh01_cnano_smart_appliance_control/firmware/pic32cm_jh01_cnano.X in MPLAB X IDE
  • Ensure PIC32CM JH01 Curiosity Nano is selected as hardware tool to program/debug the application
  • Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
  • Follow the steps in Running the Demo section

Running the Demo

Temperature Control Mode

  • The demo initializes working in Temperature Control mode. Based on the temperature measurement from Weather click, the fan speed will be controlled automatically. The LED1 on the Curiosity Nano is turned ON to indicate that the application is in Temperature Control mode.
  • The temperature reading in degree Celsius, and the fan speed will be displayed on the e-paper display. The fan speed will be indicated as follows:
    • Fan Low speed – L
    • Fan High speed – H
    • Fan Medium speed – M
    • Fan Off – OFF
  • To switch to BLE Control mode, press the touch button once. LED1 turns OFF indicating that the application has switched to BLE Control mode.
  • Once the device switches to BLE Control mode, the user can control the fan by following the steps mentioned below.
Note: Users should wait for the e-paper display to stabilize before pressing the touch button.

BLE Control Mode

  • Enable Bluetooth and Location from Smartphone settings
  • Open the Microchip Bluetooth Data (MBD) application on the smartphone and tap on the BLE UART icon on the dashboard. If prompted, allow the application to turn on Bluetooth.
  • Scan for Bluetooth devices by tapping PIC32CXBZ>SCAN>SCAN options on the MBD app
  • The RNBD device should appear as RNBD451_XXXX in the list of Bluetooth devices
  • When RNBD451_XXXX device appears, click the CANCEL button to cancel the device scanning
  • Tap on the RNBD451_XXXX device to connect to the device
  • Once the device is connected, tap on the Text mode to transfer data to device to build the communication interface between demo application and MBD app
  • Send the command FAN_ON and click Send to turn on the fan
  • User can provide the available BLE commands for this application to control the fan as desired
  • In order to return to Temperature Control mode again, user can either press the touch button again or send the BLE command TEMP_MODE. LED1 turns on again, indicating that the application has switched to Temperature Control mode.

Comments