3.6.2 Low Power Application on PIC32CM LE00 Curiosity Pro Evaluation Kit

Download

Description

The application demonstrates low power application on PIC32CM LE00 Curiosity Pro evaluation kit. On power-up, the device is set to Standby Sleep mode. The device wakes up from Standby mode and enters Active mode when the user covers the light sensor (for example, by placing a hand over it) on the I/O1 Xplained Pro Extension kit. The application periodically prints room temperature on a serial terminal while the light sensor is covered. The device goes back to Standby mode when the user uncovers the light sensor. LED0 on the PIC32CM LE00 Curiosity Pro evaluation kit is toggled every time the temperature is displayed on the serial console. When the user presses the switch SW1, the application switches Sleep mode from Standby mode to Idle mode.

Modules/Technology Used

  • Peripheral Modules
    • I2C
    • RTC
    • USART
    • DMAC
    • ADC
    • PM
    • SUPC
    • EIC
    • EVSYS

Hardware Used

Note: The application is being developed on a PIC32CM LE00 CPRO - Revision 04 evaluation kit. Ensure that the same revision on the evaluation kit is used before going further, otherwise issues with power consumption values could be faced.

Software/Tools Used

This project has been verified to work with the following versions of software tools:

Refer to the Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/pic32cm_le00_cpro.

  • Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version
  • Any Serial Terminal application, such as Tera Term terminal application

Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).

Setup

  • Connect the I/O1 Xplained Pro Extension kit to the Extension Header 1 (EXT1) of the PIC32CM LE00 Curiosity Pro evaluation kit
  • Connect a USB cable to the DEBUG USB port for programming

Programming Hex File

The pre-built hex file can be programmed by following the below steps.

Steps to program the hex file
  • Open MPLAB X IDE
  • Close all existing projects in IDE, if any project is opened
  • Go to File>Import>Hex/ELF File
  • In the Import Image File window,
    1. Create Prebuilt Project,
      • Click the Browse button to select the prebuilt hex file
      • Select Device as PIC32CM5164LE00100.
      • Ensure the proper tool is selected under Hardware Tool and click the Next button
    2. Select Project Name and Folder,
      • Select appropriate project name and folder and click the Finish button
  • In MPLAB X IDE, click the Make and Program Device button to program the device
  • Follow the steps in Running the Demo section

Programming/Debugging Application Project

  • Open the project (pic32cm_le00_cpro_low_power\firmware\pic32cm_le00_cpro.X) in MPLAB X IDE
  • Ensure PIC32CM LE00 Curiosity Pro (EDBG) is selected as hardware tool to program/debug the application
  • Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
  • Follow the steps in Running the Demo section

Running the Demo

  • Open Tera Term, connect to serial console. If there is any connection issue on tera terminal, unplug the USB cable connected to Micro-B port, and reconnect it back.
  • Change the baud rate to 115200.
  • Perform a reset by pressing the RESET switch.
  • Verify the application title message is displayed.
  • Cover the light sensor on the I/O1 Xplained Pro Extension Kit by placing the hand over it (or another element to put the light sensor in a dark environment) to print the temperature and message on the terminal. The following messages (containing the temperature value in °F) should be seen on the terminal every 500 milliseconds for the duration the light sensor is covered.
  • Observe Current Consumption on MPLAB Data Visualizer.
    Note: The MPLAB Data Visualizer is a program to process and visualize data. The MPLAB Data Visualizer can receive data from various sources, such as the Embedded Debugger Data Gateway Interface (EDBG DGI) and COM ports. It is possible to track an application in run-time using a terminal graph or oscilloscope. It analyzes the power consumption of an application through correlation of code execution and power consumption when used together with a supported probe or board.
  • Open the Data Visualizer application from the MPLAB X IDE and the PIC32CM LE00 Curiosity Pro is visible on the connection Control Panel.
  • In the MPLAB Data Visualizer tab, different interfaces will appear under the PIC32CM LE00 Curiosity Pro. Select the Power interface and click the Power Settings button. Then, click the Calibrate. After calibration is complete, click the Start Capturing Power button. A window will pop up; select Plot Raw and then click Close.
  • Ensure that the jumpers for Current Measurement on the PIC32CM LE00 Curiosity Pro are set to MEASURE for the MCU and BYPASS for the I/Os.
  • The Power Analysis window will appear on the MPLAB Data Visualizer tool interface.
  • The image shows the device in Standby mode with its measured power consumption.
    Note: The average value is considered when measuring the power consumption of the device due to the instant value is not stable. Then, the power consumption of the device in Standby mode is 8.45 µA.
  • Cover the light sensor on the I/O1 Xplained Pro Extension Kit by placing the hand over it (or another element) to print the temperature on the terminal and observe the power consumption of the device. And notice 500ms RTC timer expiry when light sensor is covered.
  • Press SW1 to switch from Standby mode to Idle mode. The following image shows the transition of the power consumption from Standby mode to Idle mode.
  • The following image shows the device in Idle mode with a measured power consumption of 138 µA.
  • Place the hand over the light sensor. The device will wake up on the next ADC window monitor interrupt, read and print data on serial and then re-enter Standby mode. The following image shows the transition of the power consumption by switching from Idle mode to Standby mode.

Comments