3.4.1 Getting Started Application on PIC32CM JH01 Curiosity Pro Evaluation Kit
Description
This application demonstrates an LED (LED0) toggle on timeout basis and print the LED toggling rate on the serial terminal. The periodicity of the timeout will change from 500 milliseconds to 1 second, 2 seconds, 4 seconds and back to 500 milliseconds every time the user presses the switch SW0 on the PIC32CM JH01 Curiosity Pro evaluation kit.
The demo application has extended functionality to read and print the current room temperature periodically when the extension header (EXT1) is plugged with the I/O1 Xplained Pro Extension kit. The temperature reading is displayed on a serial console periodically
Modules/Technology Used
- Peripheral Modules
- EIC
- RTC
- GPIO
- DMAC
- SERCOM (USART)
- SERCOM (I2C)
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer to the Project Manifest present in harmony-manifest-success.yml under
the project folder firmware/src/config/pic32cm_jh01_cpro.
- Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version
- Any Serial Terminal application, such as Tera Term/PuTTY terminal application
Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, it is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Hardware Setup 1
- Connect the PIC32CM JH01 Curiosity
Pro evaluation kit to the host PC as a USB device through a Type-A male to micro-B USB
cable connected to Micro-B USB (Debug USB) port

Hardware Setup 2
- Connect the PIC32CM JH01 Curiosity Pro evaluation kit to the host PC as a USB device through a Type-A male to micro-B USB cable connected to Micro-B USB (Debug USB) port
- To test the extended functionality,
connect the I/O1 Xplained Pro Extension Kit to the extension header EXT1
(J200) on the PIC32CM JH01 Curiosity Pro evaluation kit
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened
- Go to
File>Import>Hex/ELF File - In the Import Image File window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file
- Select Device as PIC32CM5164JH01100
- Ensure the proper tool is selected under Hardware Tool and click the Next button
- Select Project Name and Folder,
- Select appropriate project name and folder and click the Finish button
- In MPLAB X IDE, click the Make and Program Device button to program the device
- Follow the steps in Running the Demo section
- Create Prebuilt Project,
Programming/Debugging Application Project
- Open the project
(
pic32cm_jh01_cpro_getting_started/firmware/pic32cm_jh01_cpro.X) in MPLAB X IDE - Ensure
PIC32CM JH01 Curiosity Prois selected as hardware tool to program/debug the application - Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section
Running the Demo
- Open the Tera Term/PuTTY terminal application on the PC (from the Windows® Start menu by pressing the Start button)
- Set the baud rate to 115200
- An LED (LED0) on the PIC32CM JH01 Curiosity Pro evaluation kit toggles on every timeout basis and the default periodicity of the timeout is 500 milliseconds
- And, the LED toggling rate is displayed on the serial terminal
- Press the switch SW0 on the PIC32CM JH01 Curiosity Pro evaluation kit to change the default periodicity of the timeout to 1 second
- Every subsequent pressing of the switch SW0 on the PIC32CM JH01 Curiosity Pro evaluation kit changes the periodicity of the timeout to 2 seconds, 4 seconds, 500 milliseconds, and back to 1 second in cyclic order
- See the following figure for the
output.

- To Test the Extended Functionality
using I/O1 Xplained Pro Extension Kit
- Perform Hardware Setup 2 steps mentioned above, if not done already.
- Reset or power cycle the device. LED0 toggles for every 500 milliseconds during power cycle and the LED toggling rate is displayed on the serial terminal.
- Press any key on the Computer's keyboard to read and print the Temperature from the I/O1 Xplained Pro Extension kit).
- The temperature read is displayed on a serial console on a periodical basis.
- The periodicity of reading temperature will be changed between 500 milliseconds, 1 second, 2 seconds, 4 seconds, and back to 500 milliseconds every time the user presses the switch SW0 on the PIC32CM JH01 Curiosity Pro evaluation kit.
- Press any key on the keyboard to start printing the LED Toggling rate.
- The subsequent key press from the keyboard switches between printing the LED Toggling rate or temperature values on the serial terminal.
- See the following figure for the
output.

Comments
- Reference Training Module: Getting Started with Harmony v3 Peripheral Libraries on SAMC2x MCUs
- This application demo builds and
works out of box by following the instructions in Running the Demo section. If the
user needs to enhance/customize this application demo, should use the MPLAB Harmony v3
Software framework. Refer to the following links to setup and build the applications
using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232)
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253)
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project