1 Analog-to-Digital Converter (ADC) Example Component for PIC16F/18F

This document provides a guide to the MCC Melody ADC example component for PIC16F/18F microcontrollers. It covers the configuration of various peripherals, including ADC, UART, Timer, and Data Streamer. It explains how to use the MCC Melody Application Builder to add these components and configure them according to the example project. The guide includes instructions for setting up the MPLAB Data Visualizer for debugging and visualization of the ADC data. Additionally, it discusses best practices for selecting appropriate pins and addressing potential conflicts in the system configuration.

1.1 Introduction to MCC Melody Example Components

Example Components are a tight integration of learning material directly into MCC. This allows users to conveniently place configuration instructions side-by-side to the components they are configuring. For more information, refer to the MCC Melody Example Components Introduction.

Complete projects, available in MPLAB® Discover or GitHub, are specific to a board and microcontroller. However, the current project could be recreated on a range of supported microcontrollers by following the steps in the example component.

To explore what an example component is, as well as the difference between example and implementation, see MCC Melody Example Components - The Basics.

Example Components are related to MCC Melody Design Patterns for Control Flow, which shows different standard ways to organize main.c and other application-level files, such as Polling, Interrupt and Callback, or State Machine Design Patterns. Users might be familiar with each of these patterns, but...

  • What support does MCC Melody provide for each?
  • What are the recommended ways of building on the MCC Melody generated code?

1.2 MCC Melody Help Map

This diagram shows the MCC Melody Builder view, with an example project open, where links are provided for more information on a range of topics. Read the questions to find one that matches what you are looking for. The adjacent links will open online references or video training (courses) to get you familiar with different pieces of the MCC Melody and MPLAB Tools Ecosystem.

1.2.1 MCC Melody Builder, GUI

User Interface HelpMCC Melody Design Patterns for Control FlowExample ComponentsMCC Melody Technical ReferenceMCC Melody ComponentsAVR1000BPIC1000How to Write Bare Metal Code for PIC/AVR MCUsADCC API Reference, including use-casesData Streamer Library, API Reference, including use-casesUart Driver, API Reference, including use-casesTimer0 PLIB, API Reference, including use-casesADCC Example Component, running the examplesAPI References for AVR, PIC16F/18F and dsPIC, also tables of supported devices for each familyYouTube Playlist: Getting Started with MCC Melody Example ComponentsPIC18F57Q43 Datasheet

1.2.2 Tools Ecosystem Context

Where does MCC Melody fit into the MPLAB Tools Ecosystem?

Get Started Now With PIC Microcontrollers (MCUs)Get Started Now With AVR Microcontrollers (MCUs)Curiosity Nano ExplorerMPLAB X IDE Advanced Debugging (YouTube)Microchip University: MPLABX Tips and TricksMicrochip University: Visual Debugging with MPLAB Data VisualizerPIC Block Diagram - Navigation to Peripheral Tech BriefsAVR Block Diagram - Navigation to Peripheral Tech BriefsMCC Melody Data Streamer LibraryMCC Melody DV Run Time LibraryMCC Melody examples on MPLAB DiscoverMCC Melody Videos on MPLAB DiscoverMCC Melody on microchip.comMPLAB Code Configurator on microchip.comMPLAB X IDE