5 Standby Mode

The AT24C01D/AT24C02D features a low-power Standby mode that is enabled when any one of the following occurs:

  • A valid power-up sequence is performed (see Power-Up Requirements and Reset Behavior).
  • A Stop condition at the end of a valid I²C transaction is received by the device unless it initiates an internal write cycle (see Write Operations).
  • At the completion of an internal write cycle (see Write Operations).
  • An unsuccessful match of the device type identifier or hardware address in the device address byte occurs (see Device Addressing).
  • The bus host does not ACK the receipt of data read out from the device; instead, it sends a NACK response (see Read Operations).