1.2.6 Save Configuration to Project

Click on the Save Config link under a configuration (e.g., Config E) that you want to add to your project. This will open the Save Configuration to Project dialog (see figure below). If you want this to be the active configuration in the project, check the checkbox. Then click OK.

Figure 1-9. Save Configuration to Project

To open the Project Properties to see the added configuration, click the link in the Output window.

Figure 1-10. Open Project Properties from Output Window

The configuration is now added to the project. If the configuration was made active, it will also appear in the toolbar drop-down list.

Figure 1-11. Configuration Saved to Project
Note: Because the configuration has been added to the project, the Compiler Advisor will notice a change to the project properties and change Analyze to Reload.