3.3.39 UDDRC DFI Timing Register 0

Name: UDDRC_DFITMG0
Offset: 0x190
Reset: 0x07020002
Property: Read/Write

Bit 3130292827262524 
    DFI_T_CTRL_DELAY[4:0] 
Access R/WR/WR/WR/WR/W 
Reset 00111 
Bit 2322212019181716 
 DFI_RDDATA_USE_DFI_PHY_CLKDFI_T_RDDATA_EN[6:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000010 
Bit 15141312111098 
 DFI_WRDATA_USE_DFI_PHY_CLK DFI_TPHY_WRDATA[5:0] 
Access R/WR/WR/WR/WR/WR/WR/W 
Reset 0000000 
Bit 76543210 
   DFI_TPHY_WRLAT[5:0] 
Access R/WR/WR/WR/WR/WR/W 
Reset 000010 

Bits 28:24 – DFI_T_CTRL_DELAY[4:0]

Specifies the number of DFI clock cycles after an assertion or de-assertion of the DFI control signals that the control signals at the PHY-DRAM interface reflect the assertion or de-assertion. If the DFI clock and the memory clock are not phase-aligned, this timing parameter should be rounded up to the next integer value. Note that if using RDIMM/LRDIMM, it is necessary to increment this parameter by RDIMM's/LRDIMM's extra cycle of latency in terms of DFI clock.

Unit: DFI clock cycles.

Programming Mode: Quasi-dynamic Group 4

Bit 23 – DFI_RDDATA_USE_DFI_PHY_CLK 

Defines whether dfi_rddata_en/dfi_rddata/dfi_rddata_valid is generated using HDR (DFI clock) or SDR (DFI PHY clock) values.

Selects whether value in DFITMG0.dfi_t_rddata_en is in terms of HDR (DFI clock) or SDR (DFI PHY clock) cycles:

- 0 in terms of HDR (DFI clock) cycles

- 1 in terms of SDR (DFI PHY clock) cycles

Refer to PHY specification for correct value.

Programming Mode: Static

Bits 22:16 – DFI_T_RDDATA_EN[6:0]

Time from the assertion of a read command on the DFI interface to the assertion of the dfi_rddata_en signal.

Refer to PHY specification for correct value.

This corresponds to the DFI parameter trddata_en. Note that, depending on the PHY, if using RDIMM/LRDIMM, it may be necessary to use the adjusted value of CL in the calculation of trddata_en. This is to compensate for the extra cycle(s) of latency through the RDIMM/LRDIMM.

Unit: DFI clock cycles or DFI PHY clock cycles, depending on DFITMG0.dfi_rddata_use_dfi_phy_clk.

Programming Mode: Quasi-dynamic Group 1, Group 4

Bit 15 – DFI_WRDATA_USE_DFI_PHY_CLK

Defines whether dfi_wrdata_en/dfi_wrdata/dfi_wrdata_mask is generated using HDR (DFI clock) or SDR (DFI PHY clock) values.

Selects whether value in DFITMG0.dfi_tphy_wrlat is in terms of HDR (DFI clock) or SDR (DFI PHY clock) cycles

Selects whether value in DFITMG0.dfi_tphy_wrdata is in terms of HDR (DFI clock) or SDR (DFI PHY clock) cycles

- 0 in terms of HDR (DFI clock) cycles

- 1 in terms of SDR (DFI PHY clock) cycles

Refer to PHY specification for correct value.

Programming Mode: Static

Bits 13:8 – DFI_TPHY_WRDATA[5:0]

Specifies the number of clock cycles between when dfi_wrdata_en is asserted to when the associated write data is driven on the dfi_wrdata signal. This corresponds to the DFI timing parameter tphy_wrdata. Refer to PHY specification for correct value. Note, max supported value is 8.

Unit: DFI clock cycles or DFI PHY clock cycles, depending on DFITMG0.dfi_wrdata_use_dfi_phy_clk.

Programming Mode: Quasi-dynamic Group 4

Bits 5:0 – DFI_TPHY_WRLAT[5:0] Write latency

Number of clocks from the write command to write data enable (dfi_wrdata_en). This corresponds to the DFI timing parameter tphy_wrlat.

Refer to PHY specification for correct value. Note that, depending on the PHY, if using RDIMM/LRDIMM, it may be necessary to use the adjusted value of CL in the calculation of tphy_wrlat. This is to compensate for the extra cycle(s) of latency through the RDIMM/LRDIMM.

Unit: DFI clock cycles or DFI PHY clock cycles, depending on DFITMG0.dfi_wrdata_use_dfi_phy_clk.

Programming Mode: Quasi-dynamic Group 1, Group 4