Xmodem Protocol

The Send and Receive File commands use the Xmodem protocol to communicate. Any terminal using this protocol can be used to send the application file to the target. The size of the binary file to send must be lower than half the SRAM size because the Xmodem protocol requires some SRAM memory in order to work.

The Xmodem protocol supported is the 128-byte length block. This protocol uses a two-character CRC16 to ensure detection of maximum bit errors.

Xmodem protocol with CRC is supported by successful transmission reports provided both by a sender and by a receiver. Each transfer block is as follows:

<SOH><blk #><255-blk #><--128 data bytes--><checksum> in which:
  • <SOH> = 01 hex
  • <blk #> = binary number, starts at 01, increments by 1, and wraps 0FFH to 00H (not to 01)
  • <255-blk #> = 1’s complement of the blk#.
  • <checksum> = 2-byte CRC16

The following figure shows a transmission using this protocol.

Figure 2-26. Xmodem Transfer Example