3.4 Creating a New MCC Harmony Project
- To create a new project, open MPLAB X IDE and click on File>New Project
- In the “New Project” pop-up, click on Microchip Embedded>Application Project(s)>Next
- In Select Device window, select the device from drop down and click Next.
- In Select Compiler window, Select the latest compiler and click Next.
- In Select Project Name and Folder window, enter the project name and select the project location, and click Finish.
- Locate the Harmony Framework path and click Next
- Now MPLAB X Code Configurator Content
Manager will be launched automatically.
- Click on Finish
- Project Graph window of the Configurator may have predefined components.
- Project and Device resources
- Click on Finish