9.5.2 Tool Description
Zigbee OTAU Tab
The following figure provides details of this tab. Description of each button and text box is provided in the following figure:

The previous Figure 1 shows details of each button and text boxes. Details are provided for Zigbee OTAU function, Serial Port connection, UART Rx Display Box and related functions, Programming *.hex file through IPECMD.exe in this Tab. Details for item #12 and item#18 are given below
Item#12
Zigbee Update: This button is used to start the Zigbee update process
Cancel Update: This button is used to cancel Zigbee update process
Clear Devlist: clear out device list
Open The Network: send setPermitJoin 180/ invokeCommissioning 8 0 commands to open network for 180 ms
Create NewNetwork: send resetToFN command to open new network for 180 sec. Issuing this command deletes old network information in the Zigbee Server.
Item # 18
Select All: Select all items in the display box
Select Items: press Ctrl and click mouse on lines in display box to select items.
Copy Selected: Copy selected items on Clip Board
Clear: Remove all the texts from display box
Copy All: Copy all the texts from the display box
Serial Bootloader Tab
The following figure provides details of this tab. Description of each button and text box is provided in the figure.

Device can enter in Bootloader mode either through GPIO (button press) or waiting for specified amount of time after rebooting the device. Both the scenarios are handled in this tab.