1.69 CRYPT_SHA512_Finalize Function
C
int CRYPT_SHA512_Finalize(
CRYPT_SHA512_CTX* sha512,
unsigned char* digest
);
Description
This function finalizes the hash and puts the result into digest.
Preconditions
The SHA512 context must be initialized prior to calling this function. The context must not be modified by code outisde of this function.
Parameters
Parameters | Description |
---|---|
sha512 | Pointer to CRYPT_SHA512_CTX structure which holds the hash values. |
digest | Pointer to byte array to store hash result. |
Returns
BAD_FUNC_ARG - An invalid pointer was passed to the function, either in sha512 or digest.
0 - An invalid pointer was not passed to the function.
Remarks
In order to preserve the validity of the SHA512 hash, nothing must modify the context holding variable between calls to CRYPT_SHA512_DataAdd and CRYPT_SHA512_Finalize.
Example
CRYPT_SHA512_CTX sha512;
uint8_t buffer[1024];
uint8_t sha512Sum[SHA512_DIGEST_SIZE];
CRYPT_SHA512_Initialize(&sha512);
CRYPT_SHA512_DataAdd(&sha512, buffer, sizeof(buffer));
CRYPT_SHA512_Finalize(&sha512, sha512Sum);