1.60 CRYPT_SHA256_DataSizeSet Function
C
int CRYPT_SHA256_DataSizeSet(
CRYPT_SHA256_CTX* sha256,
unsigned int msgSize
);
Description
The PIC32MZ hardware encryption module needs to know the size of the data before it starts processing. This function sets that value.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
sha256 | Pointer to CRYPT_SHA256_CTX structure which holds the hash values. |
msgSize | Size of the data (in bytes) that will be processed. |
Returns
BAD_FUNC_ARG - An invalid pointer was passed to the function.
0 - An invalid pointer was not passed to the function.
Remarks
All SHA256 hashes have to start at a particular value before adding new data to it. This function sets the necessary values for the structure.
Example
CRYPT_SHA256_CTX sha256;
uint8_t buffer[1024];
uint8_t sha256sum[SHA256_DIGEST_SIZE];
CRYPT_SHA256_Initialize(&sha256);
CRYPT_SHA256DataSizeSet(&sha256, sizeof(buffer));
CRYPT_SHA256_DataAdd(&sha256, buffer, sizeof(buffer));
CRYPT_SHA256_Finalize(&sha256, sha256sum);