7 Appendix D – MCHPRT2 Tool Inbuilt Configuration
The MCHPRT2 tool comes with some of the following configuration parameters available in
the
list.ini file of the MCHPRT2 tool package, see the following
figure:- Retry function
- Module enable/disable
- DELAY – Delay between retries in milliseconds (ms). The delay range is from 0 ms to 1s.
- INIT_COUNTER – Number of retries in the initial connection loop
- FW_COUNTER – Number of retries of firmware download
- MESSAGE_DISABLE:
- MESSAGE DISABLE – 1
- MESSAGE ENABLE – 0
Note: MESSAGE ENABLE – For some decision making, the MCHPRT2 tool requests the user to manually enter a few parameters, such as, Yes or No, while executing the MCHPRT2 tool commands. For the production environment, disable the message, which is the default configuration. - Module Enable/Disable – By default, the WILC1000/WINC15x0 and the WILC3000/WINC3400 modules are enabled and SAMB11/BTLC1000 modules are disabled.