1.6 I2C Driver Asynchronous - I2C EEPROM
This example application shows how to use the I2C driver in Asynchronous mode to perform operations on the EEPROM.
Description
This example uses the I2C driver in Asynchronous mode to communicate with the EEPROM to perform write and read operations in Bare-Metal environment. This application uses I2C driver to read and write data from an AT24CM02 EEPROM device.
Downloading and Building the Application
To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/i2c/async/i2c_eeprom/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | MPLAB X project for PIC32MM USB Curiosity Development Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | PIC32MM USB Curiosity Development Board |
Setting Up PIC32MM USB Curiosity Development Board
- To run the demo, the following additional hardware is required:
- Connect micro USB cable to the USB1 connector on the board to the computer
- Install the EEPROM 3 Click board onto the mikroBUS socket J4
of PIC32MM USB Curiosity Development
BoardNote: Ensure that the series resistors on the mikroBUS headers are of value 0Ω.
Running the Application
- Build and program the application using its IDE.
- The LED is turned ON when the value read from the EEPROM matches with the written value.
| Board | LED Name |
|---|---|
| PIC32MM USB Curiosity Development Board | LED1 |