1.8 Time System Service Multi Client
This example application demonstrates the multi-client system timer functionality.
Description
For PIC32MM USB Curiosity Development Board:
- This application demonstrates timer functionality (with two clients to the Time System Service) by periodically printing a message on console every two seconds and blinking an LED every one second
- Delay, counter and single shot timer functionality is demonstrated on a switch press
- On a switch press, the application reads the current value of the 64-bit counter (say, count 1)
- It then starts a delay of 500 ms and waits for the delay to expire
- Once the delay has expired, the application again reads the current value of the 64-bit counter (say, count 2) and calculates the difference between the two counter values
- The difference count indicates the time spent for the delay and is printed on the console as, Delay time = x ms, where x is the delay value and is equal to 500 ms in the given example
- The application then starts a single shot timer of 100 ms
- When the single shot timer
expires, a message is printed on the console that says
Single shot timer of 100 ms expired - This message is printed only once on every switch press
Downloading and Building the Application
To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/system/time/sys_time_multiclient/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | MPLAB X project for PIC32MM USB Curiosity Development Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | PIC32MM USB Curiosity Development Board |
Setting Up PIC32MM USB Curiosity Development Board
- Connect micro USB cable to the USB1 connector on the board to the computer
- Install the USB UART Click board onto the mikroBUS socket J4 of PIC32MM USB Curiosity Development Board
- Connect mini USB cable to the
USB UART Click board. This will enumerate the
USB to UART port.Note: Ensure that the series resistors on the mikroBUS headers are of value 0Ω.
Running the Application
For PIC32MM USB Curiosity Development Board and PIC32 Ethernet Starter Kit:
- Open the Terminal application (e.g., Tera Term) on the computer.
- Connect to the EDBG Virtual COM
port and configure the serial settings as follows:
- Baud: 115200
- Data: 8 bits
- Parity: None
- Stop: 1 bit
- Flow Control: None
- Build and Program the application using its IDE.
- Observe the following message
getting printed on the console every two seconds.

- Press the switch and observe the
following output on the terminal (highlighted in red box).

Delay time = 500 msindicates the amount of time spent during the delaySingle shot timer of 100 ms expiredis printed only once on every switch press
- LED indicates the periodic timer
functionality:
- LED is toggled periodically every one second
| Board | Switch Name | LED Name |
|---|---|---|
| PIC32MM USB Curiosity Development Board | S1 | LED1 |