33.4 Power Management
The EVSYS can be used to wake up the CPU from a sleep mode (except Backup and Off modes), even if the clock used by the EVSYS channel and the EVSYS bus clock are disabled. Refer to the PM –Power Manager for details on the different sleep modes.
Although the clock for the EVSYS is stopped, the device still can wake up the EVSYS clock. Some event generators can generate an event when their clocks are stopped. The generic clock for the channel (GCLK_EVSYS_CHANNEL_n) will be restarted if that channel uses a resynchronized path. It does not need to wake the system from sleep.