50.1 Introduction
This chapter describes a common checklist that must be used when starting and reviewing the schematics for the PIC32CZ CA8x/CA9x design. This chapter illustrates the recommended power supply connections and how to connect the external analog references, programmer, and debugger.
Refer to the Basic 32-Bit MCU Design and Troubleshooting Checklist Guide and EMI, EMC, EFT, and ESD Circuit Design Consideration for 32-bit Microcontrollers available on the Microchip web site for more a detailed information.
- VDDIO/AVDD ≥ VDDREG during power-up or power-down.
- All capacitors are ceramic w/ESR < 1Ω.
- Package PAD must be soldered to ground with multiple via’s to ground PCB layer (see suggested PAD landing pattern).
- In the case of packages with leads, all decoupling capacitors must be placed on the same side of the PCB as the MCU and as close to the pins as possible. In the case of BGA packages, all decoupling capacitors must be placed on the opposite side of the PCB from the MCU with minimal distance between the ball and the associated capacitor.
- If USB is not being used in the application, the VUSB3V3 pins should be connected to ground.
- If JTAG will be the primary debugging interface during development or in the case that boundary scan will be implemented in manufacturing, use of any alternative functions on the TMS, TDO, TDI, and TCK pins should be avoided.
- If the trace functions are implemented, the ability to isolate these signals from any alternative functions during development is recommended.
- All ground connections must be made to the ground plane PCB layer with the shortest possible fan-out.
Option One
This ensures VDDREG will never exceed VDDIO.
This option is required for safe operation.
Option Two
This option is not recommended for safe operation.
Only approved if a soft start circuit is used on the VDDREG supply to guarantee it lags.