19.6.2 32 kHz External Crystal Oscillator (XOSC32K) Operation
The XOSC32K can operate in two different modes:
- External clock, with an external clock signal connected to XIN32
- Crystal oscillator, with an external 32.768 kHz crystal connected between XIN32 and XOUT32
At reset, the XOSC32K is disabled, and the XIN32/XOUT32 pins can either be used as General Purpose I/O (GPIO) pins or by other peripherals in the system.
When XOSC32K is enabled, the operating mode determines the GPIO usage. When in crystal oscillator mode (XOSC32K.XTALEN = 1), the XIN32 and XOUT32 pins are controlled by XOSC32K.ENABLE, and the GPIO functions are overridden on both pins. When in external clock mode (XOSC32K.XTALEN = 0), only the XIN32 pin will be overridden and controlled by XOSC32K.ENABLE, while the XOUT32 pin can still be used as a GPIO pin.
Enabling, Disabling: The XOSC32K is enabled by writing a '1' to the Enable bit in the 32 kHz External Crystal Oscillator Control register (XOSC32K.ENABLE = 1). It is necessary to wait for STATUS.XOSC32KRDY bit to set, before disabling the XOSC32K. The XOSC32K is disabled by writing a '0' to the Enable bit in the 32 kHz External Crystal Oscillator Control register (XOSC32K.ENABLE = 0). It is necessary to wait for STATUS.XOSC32KRDY to clear before enabling the XOSC32K.
Mode Selection: To enable the XOSC32K in Crystal Oscillator mode, the XTALEN bit in the 32 kHz External Crystal Oscillator Control register must be written (XOSC32K.XTALEN = 1). If XOSC32K.XTALEN is '0', the External Clock Input mode will be enabled. This bit must be written when XOSC32K.ENABLE = 0. Otherwise, the write on this bit is ignored.
Gain Selection: When a crystal oscillator is selected, a user controllable gain is provided through the CGM control bits. The user must review the electrical specification. This bit must be written when XOSC32K.ENABLE = 0. Otherwise, the write on this bit is ignored.
Startup: XOSC32K.STARTUP[3:0] selects the startup time. It is configurable and applicable for crystal mode or external clock mode. These bits must be written when XOSC32K.ENABLE = 0. Otherwise, the write on these bits is ignored.
The XOSC32K will behave differently in different sleep modes based on the settings of XOSC32K.ONDEMAND and XOSC32K.ENABLE bits. The XOSC32K.ONDEMAND bit must be written when XOSC32K.ENABLE = 0. Otherwise, the write on this bit is ignored. If XOSC32K.ENABLE = 0, the XOSC32K will be always stopped. For XOS32K.ENABLE = 1, following table is valid:
| XOSC32K.ONDEMAND | Sleep Behavior |
|---|---|
| 0 | Always run |
| 1 | Run if requested by a peripheral |
As a crystal oscillator usually requires a long start-up time, the 32 kHz External Crystal Oscillator will keep running across resets, except for Power-on Reset (POR). After a reset or when waking up from a Sleep mode where the XOSC32K was disabled, the XOSC32K will need a certain amount of time to stabilize on the correct frequency. This start-up time can be configured by changing the Oscillator Start-Up Time bit group (XOSC32K.STARTUP[3:]) in the 32 kHz External Crystal Oscillator Control register. During the start-up time, the oscillator output is masked to ensure that no unstable clock propagates to the digital logic.
Once the external clock or crystal oscillator is stable and ready to be used as a clock source, the XOSC32K Ready bit in the Status register is set (STATUS.XOSC32KRDY = 1). The transition of STATUS.XOSC32KRDY from '0' to '1' generates an interrupt if the XOSC32K Ready bit in the Interrupt Enable Set register is set (INTENSET.XOSC32KRDY = 1).