27.5 Sleep Modes

Important: To facilitate the use of sleep modes, the following conditions must be met:
  • PLL0 must be dedicated to the CPU
  • PLL0 GCLK0 must be stepped down in ≦ 75 MHz increments to ≦ 75 MHz MCLK frequency prior to entering IDLE or STANDBY sleep mode
  • PLL0 GCLK0 must be stepped up to the desired nominal operating frequency in ≦ 75 MHz maximum increments after exiting IDLE or STANDBY sleep modes
  • The GCLK0 MCLK frequency step delay for both of these processes needs to be ≧ 1 us/step

The device can be set in a sleep mode (idle, standby, hibernate, backup and off). In sleep mode, the CPU is stopped, and the peripherals are either active or idle, according to the sleep mode depth. The sleep modes and their effects on the clocks’ activity, the regulators, the power domains state, the RAMs and NVM state are described in the table and the following sections:

Table 27-3. Power Manager Sleep Modes
Sleep ModesMCLK

Main Clock

CPUAHBx/APBx

Clocks

GCLK0 clockOther GCLK clocksOscillatorsRegulatorsPower Domains StateSRAM NVM
RUNSTDBYONDEMANDLPVREGVREGSW VREGRAMVREGPLLVREGUSBPD_CORE_BUPD_CORE_SWPD_CORE_RAMPD_CORE_USBPD_CORE_PLL
ActiveRunRunRunRunRun if Requested.

(RiR)

X0RunOn (9)OnOnOn(1)ActiveActiveOn(1)ActiveActive
1RiR
IDLERunStopStop (2)RunRiRX0RunOnOnOn (1)ActiveOn(1)ActiveActive
1RiR
STANDBYRiRStopStop (2)Stop (2)Run00Run(8, 10)On (3)ActiveFull or 32 KB retention (6)On(3)(11)LPM (4)
RiR1RiR
Run10Run
RiR1RiR
HIBERNATEStopStopStopStopOff(8,10)OffOffFull or 32 KB retention (7)Off(12)Off
BACKUPStopStopStopStopOffOffOffOff
OFFOffOffOffOffOffOffOffOff
Note:
  1. Run if enabled (SUPC.VREGCTRL.AVREGENx = 0x1), or for VREGUSB, (i.e., PD_CORE_USB), only, if USB.CTRLA.ENABLE=1.
  2. Stop except if running during Sleepwalking.
  3. Run if enabled (SUPC.VREGCTRL.AVREGENx = 0x1) and run-in standby feature is enabled (SUPC.VREGCTRL.AVREGSTDBYx = 0x1).
  4. This is product specific. In some devices NVM, (Non Volatile Memory), has a separate and independent low-power configuration that is defined by NVMCTRL.CTRLB.SLEEPPRM or FCR.CTRLB.SLP if they exist.
  5. I/O are in high-impedance mode except the RESET_N pad which is still in input mode and can detect a reset to wake-up the chip.
  6. Refer to PM.STDBYCFG.RAMCFG and section: Standby Sleep Mode.
  7. Refer to PM.HIBCFG.RAMCFG and section: Hibernate Sleep Mode.
  8. The low power voltage regulator (LPVREGC) supplies the VDDCORE_BU in backup sleep mode.
  9. Behavior dependent on PM.STDBYCFG.RAMCFG.
  10. Behavior dependent on PM.HIBCFG.RAMCFG.

Idle Sleep Mode

The IDLE mode allows power optimization with the fastest wake-up time.

The CPU is stopped, the logic is retained, and peripherals are still working. Synchronous clocks are stopped except when requested. As the main clock source is still running, wake-up time is minimal. The GCLK clocks, regulators and RAM are not affected by the idle sleep mode and operates normally.

Any interrupt event for an enabled interrupt source will cause the MCU to exit IDLE mode and return to ACTIVE mode and vector to the designated interrupt service routine provided that the interrupt event is a higher priority than the current interrupt priority before entry into IDLE mode.

Table 27-4. 
USB & PLLIDLE MODE
SUPC.VREGCTRL.AVREGEN [x:y]CTRLA.ENABLE
VREGRAMLPVREGVREGSWVREGUSBnVREGPLL
VoltagePowerVoltagePowerVoltagePowerVoltagePowerVoltagePower
0x001.2vNOM0.8vNOM1.2vNOMOFF—OFF—
0x01(1)1.2vNOM0.8vNOM1.2vNOM1.2vNOMOFF—
0x301.2vNOM0.8vNOM1.2vNOM1.2vNOM1.2vNOM
0x31(1)1.2vNOM0.8vNOM1.2vNOM1.2vNOM1.2vNOM
Note:
  • USB.CTRLA.ENABLE will override USB regulator control if disabled in SUPC.VREGCTRL.AVREGEN register and force it to be enabled and active ON.

Standby Sleep Mode

The standby sleep mode is the lowest power configuration while keeping the state of the logic and the content of the RAM.

The CPU is stopped as well as the peripherals. The logic is retained, and power domain gating can be used to turn off the PD_CORE_RAM power domain fully or partially. In this mode, all clocks are stopped except those configured to perform sleepwalking tasks. The clocks can also run on request or at all times, depending on their on-demand and run-in-standby settings.

Additionally, it is possible to scale STANDBY power further with the combination use of PM.STDBYCFG.LPRAM=1 and PM.STDBYCFG.RAMCFG=1 for minimizing SRAM power consumption by powering down various SRAM sections.

Refer to the SUPC.VREGCTRL, SUPC.VREFCTRL, and PM.STDBYCFG register for more details.

Refer to Sleepwalking for more details on Sleepwalking feature.

Table 27-5. SLEEP Standby Mode MCU Power Distribution Summary
USB & PLLSTANDBY MODE
SUPC.VREGCTRL.AVREGEN [x:y]SUPC.VEGCTRL.AVREGSTDBY [x:y]
VREGRAMLPVREGVREGSWVREGUSBnVREGPLL
VoltagePowerVoltagePowerVoltagePowerVoltagePowerVoltagePower
001.2vNOM0.8vNOM1.2vNOMOFF(1)XOFF(1)X
011.2vNOM0.8vNOM1.2vNOMOFF(1)XOFF(1)X
101.2vNOM0.8vNOM1.2vNOMOFF(1)XOFF(1)X
111.2vNOM0.8vNOM1.2vNOM1.2vNOM1.2vNOM
Note:
  1. If USB.CTRLA.ENABLE=1, it will override any USB SUPC.VREGCTRL.AVREGEN regulator disable setting and force the USB regulator on.
  2. These bits are product dependent. See SUPC.VREGCTRL and SUPC.VREFCTRL registers if implemented.
Figure 27-3. System SRAM Standby Sleep Mode Extended Features

Hibernate Sleep Mode

The HIBERNATE mode allows achieving lower power consumption than STANDBY mode.

The device is entirely powered off except for:

  • The PD_CORE_BU power domain to allow few features to run (RTC, 32kHz clock sources, and wake-up from external pins)
  • The PD_CORE_RAM power domain that can be retained according to HIBCFG register configuration

All PM registers are reset to their default value when entering hibernate sleep mode except the I/O retention bit in CTRLA.IORET. If CTRLA.IORET =1, the I/O values are retained on entry and exit from HIBERNATE mode.

Table 27-6. SLEEP Hibernate Mode MCU Power Distribution Summary
USB & PLLHIBERNATE MODE
SUPC.VREGCTRL.AVREGEN [x:y]CTRLA.ENABLE
VREGRAM (1)LPVREG (2)VREGSWVREGUSBnVREGPLL
VoltagePowerVoltagePowerVoltagePowerVoltagePowerVoltagePower
XX1.2vNOM0.8vNOMOFF--OFF--OFF--
XX1.2vLOW0.8vNOMOFF--OFF--OFF--
Note:
  1. In HIBERNATE mode regulator VREGRAM is ON and supplies power to:
    • XOSC32K - 32k oscillator
    • OSCULP32K – Low Power RC
    • SUPC - Supply Controller
    • RSTC - Reset Controller
    • RTC - Real Time Clock
    • PM - Power Manager
    • TRAM – Trust RAM
    • System SRAM depending on status of PM.HIBCFG.RAMCFG which defines SRAM retention policy
  2. Low power regulator LPVREG is always on but does not supply power to any logic except in BACKUP mode.
  3. Product specific. See SUPC.VREGCTRL and SUPC.VREFCTRL registers if implemented.
Figure 27-4. SRAM Hibernate Mode Flow

Backup Sleep Mode

The BACKUP mode allows achieving the lowest power consumption aside from OFF mode.

The device is entirely powered off except for:

  • The PD_CORE_BU power domain to allow few features to run (RTC, 32kHz clock sources, and wake-up from external pins)
  • The PD_CORE_RAMρ power domain that can be retained according to HIBCFG register configuration

All PM registers are reset to their default value when entering Backup sleep mode except the I/O retention bit in CTRLA.IORET. If CTRLA.IORET =1, the I/O values are retained on entry and exit from BACKUP mode.

Table 27-7. SLEEP Backup Mode MCU Power Distribution Summary
USB & PLLBACKUP MODE
SUPC.VREGCTRL.AVREGEN [x:y]USB/PLL CTRLA.ENABLEVREGRAMLPVREG (1)VREGSWVREGUSBnVREGPLL
VoltagePowerVoltagePowerVoltagePowerVoltagePowerVoltagePower
XXOFF—0.8vNOMOFF—OFF—OFF—
Note:
  1. All regulators, other than the LPVREG regulator, are disabled and OFF and all system SRAM contents are lost In BACKUP mode only regulator LPVREG is ON and supplies power to the backup domain containing the following:
    • XOSC32K - 32k oscillator
    • OSCULP32K – Low Power RC
    • SUPC - Supply Controller
    • RSTC - Reset Controller
    • RTC - Real Time Clock
    • PM - Power Manager
    • TRAM – Trust RAM

Off Sleep Mode

The OFF mode allows achieving the lowest power consumption. The device internally is powered off and all internal regulators are disabled during OFF mode.