35.4 Peripheral Dependencies
| Peripheral Name | Base Address | NVIC IRQ Index:Source | MCLK AXI/APB Clocks Index:Name (1) | GCLK Peripheral Channel Index:Clock Name (2) | PAC Peripheral Peripheral Identifier (PAC.WRCTRL) | DMA Trigger Index:Source (DMAC.CHCTRLBk) | Power Domain |
|---|---|---|---|---|---|---|---|
| SERCOM0 | 0x4600 0000 (APB E) | 55 : ERROR; 56 : RXBRK 57 : DRE/PREC; 58 : TXC/AMATCH 59 : RXC/DRDY; 60 : RXS/SSL/TXFE 61 : CTSIC/RXFF | MCLK.CLKMSK0[31] | 18 : GCLK_SERCOM0_SLOW 21 : GCLK_SERCOM0_CORE | 23 | 5 : RX 6 : TX | VDDREG |
| SERCOM1 | 0x4600 2000 (APB E) | 62 : ERROR; 63 : RXBRK 64 : DRE/PREC; 65 : TXC/AMATCH 66 : RXC/DRDY; 67 : RXS/SSL/TXFE 68 : CTSIC/RXFF | MCLK.CLKMSK1[0] | 18 : GCLK_SERCOM1_SLOW 22 : GCLK_SERCOM1_CORE | 24 | 7 : RX 8 : TX | VDDREG |
| SERCOM2 | 0x4580 0000 (APB D) | 69 : ERROR; 70 : RXBRK 71 : DRE/PREC; 72 : TXC/AMATCH 73 : RXC/DRDY; 74 : RXS/SSL/TXFE 75 : CTSIC/RXFF | MCLK.CLKMSK1[1] | 19 : GCLK_SERCOM2_SLOW 23 : GCLK_SERCOM2_CORE | 25 | 9 : RX 10 : TX | VDDREG |
| SERCOM3 | 0x4580 2000 (APB D) | 76 : ERROR; 77 : RXBRK 78 : DRE/PREC; 79 : TXC/AMATCH 80 : RXC/DRDY; 81 : RXS/SSL/TXFE 82 : CTSIC/RXFF | MCLK.CLKMSK1[2] | 19 : GCLK_SERCOM3_SLOW 24 : GCLK_SERCOM3_CORE | 26 | 11 : RX 12 : TX | VDDREG |
| SERCOM4 | 0x4600 4000 (APB E) | 83 : ERROR; 84 : RXBRK 85 : DRE/PREC; 86 : TXC/AMATCH 87 : RXC/DRDY; 88 : RXS/SSL/TXFE 89 : CTSIC/RXFF | MCLK.CLKMSK1[3] | 18 : GCLK_SERCOM4_SLOW 25 : GCLK_SERCOM4_CORE | 27 | 13 : RX 14 : TX | VDDREG |
| SERCOM5 | 0x4580 4000 (APB D) | 90 : ERROR; 91 : RXBRK 92 : DRE/PREC; 93 : TXC/AMATCH 94 : RXC/DRDY; 95 : RXS/SSL/TXFE 96 : CTSIC/RXFF | MCLK.CLKMSK1[4] | 19 : GCLK_SERCOM5_SLOW 26 : GCLK_SERCOM5_CORE | 28 | 15 : RX 16 : TX | VDDREG |
| SERCOM6 | 0x4580 6000 (APB D) | 97 : ERROR; 98 : RXBRK 99 : DRE/PREC; 100 : TXC/AMATCH 101 : RXC/DRDY; 102 : RXS/SSL/TXFE 103 : CTSIC/RXFF | MCLK.CLKMSK1[5] | 19 : GCLK_SERCOM6_SLOW 27 : GCLK_SERCOM6_CORE | 29 | 17 : RX 18 : TX | VDDREG |
| SERCOM7 | 0x4500 0000 (APB B) | 104 : ERROR; 105 : RXBRK 106 : DRE/PREC; 107 : TXC/AMATCH 108 : RXC/DRDY; 109 : RXS/SSL/TXFE 110 : CTSIC/RXFF | MCLK.CLKMSK1[6] | 20 : GCLK_SERCOM7_SLOW 28 : GCLK_SERCOM7_CORE | 30 | 19 : RX 20 : TX | VDDREG |
| SERCOM8 | 0x4500 2000 (APB B) | 111 : ERROR; 112 : RXBRK 113 : DRE/PREC; 114 : TXC/AMATCH 115 : RXC/DRDY; 116 : RXS/SSL/TXFE 117 : CTSIC/RXFF | MCLK.CLKMSK1[7] | 20 : GCLK_SERCOM8_SLOW 29 : GCLK_SERCOM8_CORE | 31 | 21 : RX 22 : TX | VDDREG |
| SERCOM9 | 0x4500 4000 (APB B) | 118 : ERROR; 119 : RXBRK 120 : DRE/PREC; 121 : TXC/AMATCH 122 : RXC/DRDY; 123 : RXS/SSL/TXFE 124 : CTSIC/RXFF | MCLK.CLKMSK1[8] | 20 : GCLK_SERCOM9_SLOW 30 : GCLK_SERCOM9_CORE | 32 | 23 : RX 24 : TX | VDDREG |
|
Note:
| |||||||
I/O Lines
Using the SERCOM I/O lines requires the I/O pins to be configured using port configuration (PORT). The SERCOM has four internal pads, PAD[3:0], and the signals from I2C, SPI and USART are routed through these SERCOM pads through a multiplexer. The configuration of the multiplexer is available from the different SERCOM modes. Refer to the mode specific sections below for additional information.
Power Management
The SERCOM can operate in any Sleep mode provided the selected clock source is running. SERCOM interrupts can be configured to wake the device from sleep modes.
Clocks
The SERCOM bus clock (CLK_SERCOMx_APB) can be enabled and disabled in the Main Clock Controller. The SERCOM APB BUS interface clocks are enabled by default on reset.
The SERCOM uses two generic clocks: GCLK_SERCOMx_CORE and GCLK_SERCOMx_SLOW. The core clock (GCLK_SERCOMx_CORE) is required to clock the SERCOM while working as a host. The slow clock (GCLK_SERCOMx_SLOW) is only required for certain functions. See specific mode sections below for details.
These clocks must be configured and enabled in the Generic Clock Controller (GCLK) before using the SERCOM.
The generic clocks are asynchronous to the user interface clock (CLK_SERCOMx_APB). Due to this asynchronicity, writing to certain registers will require synchronization between the clock domains. Refer to Synchronization for details.
DMA
The DMA request lines are connected to the DMA Controller (DMAC). The DMAC must be configured before the SERCOM DMA requests are used.
Concurrent DMA and CPU accesses to the DATA register must be avoided, as this may lead to unpredictable behavior.
Debug Operation
- USART.DBGCTRL
- SPI.DBGCTRL
- I2C Host DGBCTRL
Register Access Protection
All registers with write access can be write-protected optionally by the Peripheral Access Controller (PAC), except for the following registers:
- Interrupt Flag Clear and Status register (INTFLAG)
- Status register (STATUS)
- Data register (DATA)
- Address register (ADDR)
Optional write protection by the Peripheral Access Controller (PAC) is denoted by the "PAC Write Protection" property in each individual register description.
PAC write protection does not apply to accesses through an external debugger.