17.3.3 Environment Setup
The following steps outline how to set up the environment:
- The user must extract the EV79Y91A package folder.
- Inside the EV79Y91A package folder, locate the
install.shscript. - Double-click the
install.shto run the script. - The
install.shscript generates the Harmony 3 (H3) folder repository.Figure 17-5. Creating H3 Folder - After executing the
install.shscript from the EV79Y91A package folder, it clones all the required H3 repositories. Following this, the H3 repository environment becomes available within the EAP package at \EV79Y91A\H3.Figure 17-6. H3 Repositories - Open the MPLAB® X IDE, then add the Harmony Content Path. Go to Tools>Options>Plugins.
Figure 17-7. Harmony Content Path Note: The Harmony Content Path varies depending on the user’s folder structure. - Click Apply, then Click OK.Note: The user must restart the MPLAB X IDE tool.