4.7.4.5 User Application Development
This section talks about the mandatory code modifications that need to be incorporated in order to implement the sleep mode functionality.
- Include
definitions.hin all the files where UART will be used to print debug information.
definitions.h is not specific to just UART peripheral, instead it must
be included in all application source files where peripheral functionality will be
exercised.- Step 1:
app_user_edits.c- Some of the Harmony 3 generated files
cannot be fully configured by the MPLABX Code Configurator. This file contains the
instructions for the user to modify these files.
Follow the instruction mentioned on the app_user_edits.c file and after completing the required edits, comment out or remove the #error line. Also see 14.1 User Action.
- Some of the Harmony 3 generated files
cannot be fully configured by the MPLABX Code Configurator. This file contains the
instructions for the user to modify these files.
- Step 2:
zigbeeAppDeviceSelect.h- Default Generated: “#define CS_UID 0 //Unique Identifier (UID) determining the device extended address”.
- Change to a unique value: “#define CS_UID 0x123bee //Unique Identifier (UID)
determining the device extended address”.
Reason: By default, the coordinator also has the same value. In a network the UID value should be unique.
Note: The below modifications are specific to the Deep Sleep mode feature.
- Step 3:
stackConfig.h(optional)If the deep sleep period has to be increased/decreased according to the requirements, then it has to be changed in the
stackConfig.hfile as mentioned below.Make sure that the “CS_DEFAULT_END_DEVICE_TIMEOUT” value should be three times greater than the “CS_END_DEVICE_SLEEP_PERIOD”. For example, if the Device deep sleep period is 1 min, then the End device timeout period should be greater than 3 min.
Related Links
4.7.3 Zigbee Centralized Network Formation by Combined Interface