7.2.3 RFD Project Verification
LED indications :
In the RFD the following are the different led combinations indicating the following activity:
- If the blue led is constantly ON and Red led BLINKS in RGB LED - it means the RFD is not commissioned. This situation also arises if a commissioned RFD is powered off and powered on again.
- If quick green flash of the RGB LED in RFD indicates the reception of a queued data from the coordinator.
- A quick blue flash of User-LED indicates a push data was sent from RFD to the coordinator.
The output generated by the End-device in the Push Pull Star application.
End-device 1
End-device 2
End-device 3
End-device 4