4.7.3.5 User Application Development
- Build Project, upon building project user action is required as mentioned 14.1 User Action.
definitions.hin all the files where UART will be used to print debug information.Note:definitions.his not specific to just UART peripheral, instead it must be included in all application source files where peripheral functionality will be exercised.- Edit device unique ID
(
zigbeeAppDeviceSelect.h).All the Zigbee devices/modules will hold their unique IEEE address purchased from IEEE. For the demo purpose, where UID is not present in internal NVM, the pre-compiled fixed UID to be used. Edit the CS_UID to user defined value and not matching with combined interface UID (default 0xbee) as below in
zigbeeAppDeviceSelect.h. - Optional files:
app_button_handler.candapp_button_handler.hare located in<Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\zigbee\combinedInterface\firmware\srcfolder. These files enable proper button functionality. Users can add these files to their project or utilize them to create other functionalities.