1.4 I2C Driver Asynchronous - I2C EEPROM
This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM.
Description
This example uses the I2C driver in asynchronous mode to communicate with the EEPROM to perform write and read operations in Bare-Metal environment. This application uses I2C driver to read and write data from an AT24CM02 EEPROM device.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/i2c/async/i2c_eeprom/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_rh71_ek.X | MPLABX project for SAM RH71 Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_rh71_ek.X | SAM RH71 Evaluation Kit |
Setting Up SAM RH71 Evaluation Kit
- To run the demo, the following additional hardware are required:
- One EEPROM 3 Click board
- One mikroBUS Xplained Pro boards
- Connect mikroBUS Xplained Pro board to J24 header
- Plug the EEPROM 3 click Board into the mikroBUS socket of the mikroBUS Xplained Pro board
- Connect the J15 USB port on the board to the computer using a mini USB cable
- Connect debugger to the 20-pin JTAG header J33
Running the Application
- Build and program the application using its IDE
- LED indicates success or failure:
- The LED is turned ON when the value read from the EEPROM matched with the written value
| Board | LED Name |
|---|---|
| SAM RH71 Evaluation Kit | LED0 |