1 Harmony 3 Driver and System Service Application Examples for SAM RH71 Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
| Name | Description |
|---|---|
| FAT Filesystem using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FAT Filesystem using SDSPI Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
| FreeRTOS Task Notification | This example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore |
| I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
| I2C Driver Synchronous - I2C EEPROM | This example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM |
| Parallel PROM SST38 Driver - SST38VF6401 Memory Read Write | This example application shows how to use the Parallel PROM SST38 driver to perform read and write operations on a SST38VF6401 memory |
| Parallel PROM SST39 Driver - SST39VF040 Memory Read Write | This example application shows how to use the Parallel PROM SST39 driver to perform read and write operations on a SST39VF040 memory |
| SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
| SPI Driver Synchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment |
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
| USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |