12.11.4 Changing the Maximum PCIe Data Rate Settings for Connector
The Maximum PCIe Data Rate displays the maximum PCIe data rate between the controller and
the drives connected to the connector. This setting allows to change the maximum PCIe
data rate of the connector on Adaptec Smart Storage Controller. The supported values are
PCIe 3.0, PCIe 4.0, and PCIe 5.0.
Note: The maximum PCIe data rate
will be displayed only if it is supported by the controller. A reboot is required
for the new maximum PCIe data rate to take effect.
To change the Maximum PCIe Data Rate settings from the connector level:
- In the Enterprise View, select a connector.
- On the ribbon, in the Controller
group, click Set Properties.

The Set Properties window opens.
- From the Maximum PCIe
Data Rate drop-down list, change the maximum PCIe data rate
setting for the connector to PCIe 3.0, PCIe 4.0, or PCIe 5.0.

- Click OK.
- Reboot the server.