3.5.2 Software Configuration
No software configuration is required to program and debug the same device that is mounted on the board.
To program and debug a different microcontroller than what is mounted on the board, Atmel Studio must be configured to allow free selection of devices and programming interfaces.
- Navigate to through the menu system at the top of the application.
- Select the category in the options window.
- Set the Hide unsupported devices option to False.
 
        Info:  Atmel
            Studio allows any microcontroller and interface to be selected when Hide unsupported
                devices is set to False, also microcontrollers and interfaces which are
            not supported by the on-board debugger.