Introduction
The ATA8352 UWB device is a new, low-power, Ultra-Wideband (UWB) transceiver based on the ATA8350 UWB device with an integrated security layer for secure distance bounding, localization and point-to-point data communication. The digital transmitting circuity of the ATA8352 UWB device ensures maximum flexibility in the generation of UWB pulse signals.
In addition, this application note provides details about the
following:
- The migration from the ATA8350 to ATA8352 UWB device.
- The major feature differences between the ATA8350 and ATA8352 devices along with the new additional features.
- An explanation of removing old features and their impacts to the user application.