1.14 FLEXCOM RS485

This example application shows how to use the FLEXCOM module in RS485 mode.

Description

This example connects two boards through the RS485 interface.

One board acts as the transmitter, and the other acts as the receiver.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/flexcom/flexcom_rs485/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_9x60_curiosity.XMPLABX project for SAM9X60 Curiosity Development Board

Setting Up AT91Bootstrap Loader

To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_9x60_curiosity.XSAM9X60 Curiosity Development Board

Setting Up SAM9X60 Curiosity Development Board

ADDTIONAL HARDWARE REQUIRED
SETTING UP THE BOARD
  • Connect a programming cable from JTAG connector J12 on board to programmer(J-32 Debugger)
  • Connect programmer(J-32 Debugger) to computer using a micro USB cable
  • Connect the USB port J1 on board to the computer using a micro USB cable (to power the board)
  • The hardware setup requires two boards, one acting as the Host and the other as the Client
  • Connect the RX485-XPRO to the mikroBUS socket on the board using wires, following the table below
    ATRS485 J100mikroBUS 1SAM9X60
    UART_TX IO014MOSIPA22 FLEX5_IO0
    UART_RX IO113MISOPA21 FLEX5_IO1
    UART RTS IO45SDAPA00 FLEX5_IO4
    3.3V203.3V3.3V
    GND2 or 19GNDGND

Running the Application

  1. Open the Terminal application (Ex.:Tera term) on the computer.
  2. Connect to the USB Serial COM port and configure the serial settings as follows:
    • Baud: 115200
    • Data: 8 Bits
    • Parity: None
    • Stop: 1 Bit
    • Flow Control: None
  3. Build and Program the application using its IDE.
  4. One board acts as the transmitter, and the other acts as the receiver.

    This is defined by the user.