Introduction
This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Frequency Meter functionality.
The following driver API modes are covered by this manual:
Polled APIs
Callback APIs
The following peripheral is used by this module:
FREQM (Frequency Meter)
The following devices can use this module:
Atmel | SMART SAM L22
Atmel | SMART SAM C20
Atmel | SMART SAM C21
The outline of this documentation is as follows: