35.2.6.3 Transfer Counter in Client Mode
In Client mode, the transfer counter will still decrement as data is shifted in and out of the SPI module, but it will not control data transfers. The BMODE bit along with the transfer counter is used to determine when the device will look for Client Select faults.
When BMODE = 0
, the SSFLT bit will be
set if Client Select transitions from its Active to Inactive state during bytes of data
or if it transitions before the last bit sent during the final byte (if SPIxTWIDTH ≠
0
).
When BMODE = 1
, the SSFLT bit will be set if Client Select transitions
from its Active to Inactive state before the final bit of each individual transfer is
completed.