35.3.1 Full Duplex Mode
When BMODE = 1
, data transfers will occur whenever the receive FIFO is
not full and data is present in the transmit FIFO. In practice, as long as the receive
FIFO is not full, data will be transmitted/received as soon as the SPIxTXB register is
written to, matching the functionality of SPI (MSSP) modules on older 8-bit Microchip
devices. The SPIxTCNT will decrement with each transfer. However, when SPIxTCNT is zero,
the next transfer is not inhibited and the corresponding SPIxTCNT decrement will cause
the count to roll over to the maximum value. The following figure shows an example of a
communication using this mode.
1
, TXR = 1
When BMODE = 0
, the transfer counter (SPIxTCNT) must also be written to
before transfers will occur. Transfers will cease when the transfer counter reaches
‘0
’. For example, if SPIxTXB is written twice and then SPIxTCNTL is
written with ‘3
’, the transfer will start with the SPIxTCNTL write. The
two bytes in the TXFIFO will be sent after which the transfer will suspend until the
third and last byte is written to SPIxTXB.