2.4 Electric Parameters
Input Voltage
Main power supply input: DC 24V ~ 48V
Driver power supply input: 12V
Phase Current
The phase current is constrained by the rated current , which defines the maximum current that can be endured by the driver board.
A current bigger than can cause damage on the driver board.
DC Bus Current
The DC bus current is constrained by the over-current (OC) threshold .
is the smallest transient DC bus current which triggers the over-current event on the control board. depends on the shunt resistance on the driver board and the OC circuit on the control board. The control board triggers an OC event if the regulated signal is not less than ; and the regulated signal is , therefore:
.
Where,
is the shunt resistance for the DC bus current
is the regulating circuit’s gain for the DC bus current sample signal
AVDD is the analog power supply voltage for the ADC
and AVDD are fixed for a certain control board, while can be modified by the user. In other words, can be defined by the user by selecting .
is recommended to be selected in such a manner that is not bigger than .