5 Using TCB in Sleep Mode
Use case description: Configure TCB to generate an overflow interrupt every second, even when the microcontroller is in Standby sleep mode, and toggle a GPIO pin (PB5).
Result: TCB overflow interrupt will be triggered every one second, regardless of the running mode of the microcontroller (Idle/Standby). In the Interrupt Service Routine (ISR), the on-board LED, corresponding to PB5, will be toggled.
TCBn is by default disabled in Standby sleep mode; as soon as the microcontroller enters
sleep mode, TCB will be halted. The module can stay fully operational in Standby sleep
mode if the Run In Standby (RUNSTDBY) bit in the TCBn.CTRLA register is written to
‘1’.
Configuring the System Clock for Sleep Mode
To obtain an interrupt of one second for the 16-bit TCB timer, the input frequency must be as low as possible. For this, the internal 32 kHz oscillator can be used. There is no need to use a frequency divider, so the prescaler for CLK_PER must be disabled. There are three steps in the configuration process:
- Disable the CLK_PER
prescaler - The following code snippet will demonstrate how to
disable the CLK_PER
prescaler.
ccp_write_io( (void *) &CLKCTRL.MCLKCTRLB , (0 << CLKCTRL_PEN_bp)); - Select the internal 32 kHz
oscillator - The following code snippet will switch the system clock
source to the internal 32 kHz
oscillator.
ccp_write_io( (void *) &CLKCTRL.MCLKCTRLA, (CLKCTRL_CLKSEL_OSCULP32K_gc));
- Wait for the clock switch
process to complete - The following code snippet will demonstrate
how to wait for the clock source switching process to
finish.
while (CLKCTRL.MCLKSTATUS & CLKCTRL_SOSC_bm) { ; }
Configuring the Sleep Mode Operation
Sleep modes are used to shut down peripherals and clock domains in the device to save power. The Sleep Controller (SLPCTRL) controls and handles the transitions between Active and sleep mode. Four modes are available: One Active mode in which software is executed and three sleep modes. The available sleep modes are Idle, Standby, and Power-Down.
SLEEP instruction. The TCB module can run while the microcontroller is in Standby sleep mode. The Power-Down sleep mode disables TCB completely.
SLEEP instruction is
executed.SLPCTRL.CTRLA = SLPCTRL_SMODE_gm | SLPCTRL_SMODE_STDBY_gc;
Configuring TCB in Periodic Interrupt Mode
- TCBn.CCMP
- TCBn.CTRLA
The TCB Capture/Compare register must be loaded with a comparison value which will
trigger an interrupt. For this document, a value of one second for the periodic
interrupt has been chosen. With an input frequency of 32.768 kHz, the 16-bit counter
will make a complete cycle in two seconds (the maximum value of a 16-bit number is
65535). Since the maximum value the 16-bit TCB counter can achieve is 65535 for the
two seconds maximum period, the CCMP register must be loaded with half of the
maximum value – 32768 (0x7FFF). The following code snippet loads
the TCB0.CCMP register with 0x7FFF.
TCB0.CCMP = 0x7fff;
Prescaling is not needed, so the divider value will be ‘0’. Also,
the timer must be enabled. For the TCB to still generate an interrupt while in
Standby sleep mode, the RUNSTDBY bit must also be enabled. The following code
snippet sets the clock divider to ‘0’, enables the timer, and
allows the timer to run in Standby sleep mode.
TCB0.CTRLA = TCB_CLKSEL_CLKDIV1_gc | TCB_ENABLE_bm | TCB_RUNSTDBY_bm;
To trigger a periodic interrupt, the CAPT bit of the TCB0.INTCTRL register must be enabled. The following code snippet enables the interrupt.
TCB0.INTCTRL = TCB_CAPT_bm;
- The global interrupts must be also enabled. This can be done at a later step in the software program.
- All operations are halted in Power-Down sleep mode.
Configuring a Pin as Output for Visualizing Interrupt Occurrence
To visualize the periodic interrupt occurrence, the PB5 pin will be configured in Output mode. The following code sets PB5 as output low.
PORTB_DIR |= PIN5_bm; PORTB_OUT |= PIN5_bm;
An MCC generated code example for AVR128DA48, with the same functionality as the one described in this section, can be found here: