3.6.9 PolarFire Video Kit Setup Instructions
(Ask a Question)3.6.9.1 Introduction to PolarFire Video Kit Setup Instructions
(Ask a Question)These instructions describe how to setup, compile and run an example on the PolarFireVideo Kit with the MiV_RV32 Reference Design. The instructions below assume your host computer is running Linux, but similar steps can be done on Windows.
3.6.9.2 PolarFire® Video Kit Image
(Ask a Question)
3.6.9.3 Board Connections
(Ask a Question)The following cables must be connected to the board for use with SmartHLS :
- Power cable (connects to
12V Power Supply Input
). - Mini-USB cable for serial communication to the board and embedded JTAG programmer. The same cable is used for both. Alternatively, you use the External FP6 programmer.
- Jumper
J28
must be open to use the external programmer, or closed to use the embedded programmer.
3.6.9.4 Install Host PC Applications
(Ask a Question)The following programs are required to be installed on the host PC to set up the PolarFire Video Kit:
- SmartHLS v2023.2 or newer.
- Libero v2023.2 or newer.
- SoftConsole v2021.3 or later.
- A serial communication terminal of your choosing. in this guide we will use tio.
3.6.9.5 Write, compile and run a simple test program
(Ask a Question)During the test we will open the 3 serial terminals labeled below:
UART Terminal
: We will use this to see the stdout from the program.SmartHLS terminal
: Linux terminal that we will use this to run SmartHLS commands from the command-line.OpenOCD terminal
: Linux terminal that we will use this to launch OpenOCD manually from the command-line.
Create a temporary directory, for example, test
, and use your favorite text editor to write the following 4 files under this directory:
$> mkdir test $> cd test
Create a simple_add.c
file with the following content:
#include <stdio.h> #include <stdint.h> uint32_t hw_add(uint32_t a, uint32_t b) { #pragma HLS function top #pragma HLS interface default type(axi_target) return a + b; } int main() { uint32_t sum; uint32_t a = 2, b = 3; sum = hw_add(a, b); int error = (sum != a + b); printf("\n%s\n", error ? "FAIL" : "PASS"); return error; }
Create the Makefile
with the following content:
NAME=simple_add SRCS=$(NAME).c LOCAL_CONFIG = -legup-config=config.tcl LEVEL = $(SHLS_ROOT_DIR)/examples include $(LEVEL)/Makefile.common
Create a config.tcl
file:
source $env(SHLS_ROOT_DIR)/examples/legup.tcl set_project PolarFire MPF300 MiV_SoC
Create a gdb.txt
file with the following instructions for gdb to connect to OpenOCD, load the .elf binary into the MiV_RV32’s memory and run the code:
set $target_riscv = 1
set mem inaccessible-by-default off
set arch riscv:rv32
target extended-remote localhost:3333
load
run
Note that we used the SHLS_ROOT_DIR
environment variable, it should point to where SmartHLS is installed. On the SmartHLS Terminal
type the following:
$> export SHLS_ROOT_DIR=/path/to/Microchip/SmartHLS_2024.2/SmartHLS
Now run the SmartHLS SoC flow to:
- Compile the
hw_add
function into a Verilog module - Integrate the module into the MiV_RV32 Reference Design. See MiV_RV32 Reference Design
- Run RTL synthesis
- Run place and route
- Check timing
- Program the FPGA
The command below will invoke all these tasks as they are dependencies to program the FPGA. This will take a few minutes:
$> shls -a soc_accel_proj_program
Now cross-compile the simple_add.c
program. This will generate a hls_output/simple_add.elf
file.
$> shls soc_sw_compile_accel
In the UART terminal
open the UART connection. Your device may be different:
$> tio /dev/ttyUSB0 -b 115200
In the OpenOCD terminal
launch OpenOCD.
$> openocd -f board/microsemi-riscv.cfg
Now go back to the SmartHLS terminal
and run gdb to execute the code on the MiV_RV32.
$> riscv64-unknown-elf-gdb ./hls_output/simple_add.elf -x ./gdb.txt
At this point you should see the word PASS
in the UART terminal
. You can type Ctrl+C
and then press q
to terminate the gdb session.
Also, you can press Ctrl+C
on the OpenOCD terminal
to close the program, otherwise it would not release the JTAG cable.