When you right click an item in one of the tabs in the Main Object
Browser, you can choose from available options, which can include placing an item to a
location, unplacing an item from a location, locking the placement, and assigning a
region.
Multiple items can be selected and assigned to the same region at the same
time. You can also select a region assignment by right clicking an item and choosing Region Assign. The dialog box opens as shown in the following
figure. This option is not available for objects in the Region tab.
Figure 9-40. Select Region Dialog Box
The progress of All Region Assign and Unassign commands is as shown in
the following figure. Figure 9-41. Progress of All Region Assign
and Unassign Commands
Note: This dialog shows only the progress, and does not allow
the user to cancel the operation. Closing the dialog does not terminate the
operation.