16.3.1 All Macros
(Ask a Question)16.3.1.1 AND2
(Ask a Question)Inputs | Output |
---|---|
A, B | Y |
A | B | Y |
---|---|---|
X | 0 | 0 |
0 | X | 0 |
1 | 1 | 1 |
16.3.1.2 AND3
(Ask a Question)Input | Output |
---|---|
A, B, C | Y |
A | B | C | Y |
---|---|---|---|
X | X | 0 | 0 |
X | 0 | X | 0 |
0 | X | X | 0 |
1 | 1 | 1 | 1 |
16.3.1.3 AND4
(Ask a Question)Input | Output |
---|---|
A, B, C, D | Y |
A | B | C | D | Y |
---|---|---|---|---|
X | X | X | 0 | 0 |
X | X | 0 | X | 0 |
X | 0 | X | X | 0 |
0 | X | X | X | 0 |
1 | 1 | 1 | 1 | 1 |
16.3.1.4 CFG1/2/3/4 and Look-Up Tables (LUTs)
(Ask a Question)CFG1, CFG2, CFG3, and CFG4 are post-layout LUTs that implement any 1-input, 2-input, 3-input, and 4-input combinational logic functions respectively. Each of the CFG1/2/3/4 macros has an INIT string parameter that determines the logic functions of the macro. The output Y is dependent on the INIT string parameter and the values of the inputs.
16.3.1.5 CFG2
(Ask a Question)Input | Output |
---|---|
A,B | Y = f (INIT, A, B) |
BA | Y |
---|---|
00 | INIT[0] |
01 | INIT[1] |
10 | INIT[2] |
11 | INIT[3] |
16.3.1.6 CFG3
(Ask a Question)Input | Output |
---|---|
A, B, C | Y = f (INIT, A,B, C) |
CBA | Y |
---|---|
000 | INIT[0] |
001 | INIT[1] |
010 | INIT[2] |
011 | INIT[3] |
100 | INIT[4] |
101 | INIT[5] |
110 | INIT[6] |
111 | INIT[7] |
16.3.1.7 CFG4
(Ask a Question)Input | Output |
---|---|
A, B, C, D | Y = f (INIT, A,B, C, D) |
DCBA | Y |
---|---|
0000 | INIT[0] |
0001 | INIT[1] |
0010 | INIT[2] |
0011 | INIT[3] |
0100 | INIT[4] |
0101 | INIT[5] |
0110 | INIT[6] |
0111 | INIT[7] |
1000 | INIT[8] |
1001 | INIT[9] |
1010 | INIT[10] |
1011 | INIT[11] |
1100 | INIT[12] |
1101 | INIT[13] |
1110 | INIT[14] |
1111 | INIT[15] |
16.3.1.8 BUFF
(Ask a Question)Buffer.
Input | Output |
---|---|
A | Y |
A | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.9 BUFD
(Ask a Question)Input | Output |
---|---|
A | Y |
A | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.10 BUFD_DELAY
(Ask a Question)Input | Output |
---|---|
A | Y |
A | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.11 CLKINT
(Ask a Question)Input | Output |
---|---|
A | Y |
A | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.12 GBR
(Ask a Question)Back-annotated macro that routes an internal fabric signal to global network.

Input | Output |
---|---|
An | Y |
An | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.13 CLKINT_PRESERVE
(Ask a Question)Input | Output |
---|---|
A | Y |
A | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.14 GRESET
(Ask a Question)This Macro connects an I/O or route an internal fabric signal to the global reset network. The connection to the GRESET is hardened for radiation only if the driver is an I/O fixed at a package pin with GRESET in its function name. Routing an internal fabric signal through the GRESET macro is hardened by the radiation.
A | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.15 RCLKINT
(Ask a Question)This Macro routes an internal fabric signal to a row global buffer, thus creating a local clock.

Input | Output |
---|---|
A | Y |
A | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.16 RGB
(Ask a Question)Back-annotated macro that routes an internal fabric signal to a row global buffer.
Input | Output |
---|---|
An | YL, YR |
An | YL | YR |
---|---|---|
0 | 0 | 0 |
1 | 1 | 1 |
16.3.1.17 RGRESET
(Ask a Question)Macro used to route a triplicated fabric signal to a row global buffer and create a local reset. The three input bits must be driven by three separate logic cones replicating the paths from the source registers.

A[2] | A[1] | A[0] | Y |
---|---|---|---|
X | 0 | 0 | 0 |
0 | X | 0 | 0 |
0 | 0 | X | 0 |
X | 1 | 1 | 1 |
1 | X | 1 | 1 |
1 | 1 | X | 1 |
16.3.1.18 SLE
(Ask a Question)Sequential Logic Element.
Input | Output | |
---|---|---|
Name | Function | Name |
D | Data input | Q |
CLK | Clock input | |
EN | Active-High CLK enable | |
ALn | Asynchronous Load. This active-low signal either sets the register or clears the register depending on the value of ADn. | |
ADn1 | Static asynchronous load data. When ALn is active, Q goes to the complement of ADn. | |
SLn | Synchronous load. This active-low signal either sets the register or clears the register depending on the value of SD, at the rising edge of the clock. | |
SD1 | Static synchronous load data. When SLn is active (that is, low), Q goes to the value of SD at the rising edge of CLK. | |
LAT1 | LAT is always tied to low. Q output is invalid when LAT=1. |
- ADn, SD, and LAT are static signals defined at design time and need to be tied to 0 or 1.
ALn | ADn | LAT | CLK | EN | SLn | SD | D | Qn+1 |
---|---|---|---|---|---|---|---|---|
0 | ADn | X | X | X | X | X | X | !ADn |
1 | X | 0 | Not rising | X | X | X | X | Qn |
1 | X | 0 | ↑ | 0 | X | X | X | Qn |
1 | X | 0 | ↑ | 1 | 0 | SD | X | SD |
1 | X | 0 | ↑ | 1 | 1 | X | D | D |
X | X | 1 | X | X | X | X | X | Invalid |
16.3.1.19 SLE_RT
(Ask a Question)Sequential Logic Element macro available only in post-layout netlist.

Input | Output | |
---|---|---|
Name | Function | Q |
D | Data input | |
CLK | Clock input | |
EN | Active High CLK enable | |
ALn | Asynchronous Load. This active low signal either sets the register or clears the register depending on the value of ADn. | |
ADn1 | Static asynchronous load data. When ALn is active, Q goes to the complement of ADn. | |
SLn | Synchronous load. This active low signal either sets the register or clears the register depending on the value of SD, at the rising edge of the clock. | |
SD1 | Static synchronous load data. When SLn is active (that is, low), Q goes to the value of SD at the rising edge of CLK. | |
DELEN1 | Enable Single-event Transient mitigation. |
- ADn, SD, and DELEN are static signals defined at design time and need to be tied to 0 or 1.
ALn | ADn | CLK | EN | SLn | SD | D | Qn+1 |
---|---|---|---|---|---|---|---|
0 | ADn | X | X | X | X | X | !ADn |
1 | X | Not rising | X | X | X | X | Qn |
1 | X | ↑ | 0 | X | X | X | Qn |
1 | X | ↑ | 1 | 0 | SD | X | SD |
1 | X | ↑ | 1 | 1 | X | D | D |
16.3.1.20 ARI1
(Ask a Question)The ARI1 macro is responsible for representing all arithmetic operations in the pre-layout phase.

Input | Output |
---|---|
A, B, C, D, FCI | Y, S, FCO |
The ARI1 cell has a 20 bit INIT string parameter that is used to configure its functionality. The interpretation of the 16 LSB of the INIT string is shown in the following table. F0 is the value of Y when A = 0 and F1 is the value of Y when A = 1.
ADCB | Y | |
---|---|---|
0000 | INIT[0] | F0 |
0001 | INIT[1] | |
0010 | INIT[2] | |
0011 | INIT[3] | |
0100 | INIT[4] | |
0101 | INIT[5] | |
0110 | INIT[6] | |
0111 | INIT[7] | |
1000 | INIT[8] | F1 |
1001 | INIT[9] | |
1010 | INIT[10] | |
1011 | INIT[11] | |
1100 | INIT[12] | |
1101 | INIT[13] | |
1110 | INIT[14] | |
1111 | INIT[15] |
Y | FCI | S |
---|---|---|
0 | 0 | 0 |
0 | 1 | 1 |
1 | 0 | 1 |
1 | 1 | 0 |
ARI1 LOGIC
[Required-Cleanup]:The 4 MSB of the INIT string controls the output of the carry bits. The carry is generated using carry propagation and generation bits, which are evaluated according to the following tables.
INIT[17] | INIT[16] | G |
---|---|---|
0 | 0 | 0 |
0 | 1 | F0 |
1 | 0 | 1 |
1 | 1 | F1 |
INIT[19] | INIT[18] | P |
---|---|---|
0 | 0 | 0 |
0 | 1 | Y |
1 | X | 1 |
P | G | FCI | FCO |
---|---|---|---|
0 | G | X | G |
1 | X | FCI | FCI |
16.3.1.21 ARI1_CC
(Ask a Question)
Input | Output |
---|---|
A, B, C, D, CC | Y, S, P, UB |
The ARI1_CC cell has a 20-bit INIT string parameter that is used to configure its functionality. The interpretation of the 16 LSB of the INIT string is shown in the following table. F0 is the value of Y when A = 0 and F1 is the value of Y when A = 1. The following table shows the interpretation of 16 LSB of the INIT string for AR1_CC.
ADCB | Y | |
---|---|---|
0000 | INIT[0] | F0 |
0001 | INIT[1] | |
0010 | INIT[2] | |
0011 | INIT[3] | |
0100 | INIT[4] | |
0101 | INIT[5] | |
0110 | INIT[6] | |
0111 | INIT[7] | |
1000 | INIT[8] | F1 |
1001 | INIT[9] | |
1010 | INIT[10] | |
1011 | INIT[11] | |
1100 | INIT[12] | |
1101 | INIT[13] | |
1110 | INIT[14] | |
1111 | INIT[15] |
The 4 MSB of the INIT string controls the output of the carry bits. The carry is generated using carry propagation and generation bits, which are evaluated according to the following tables.
INIT[17] | INIT[16] | UB |
---|---|---|
0 | 0 | 1 |
0 | 1 | !F0 |
1 | 0 | 0 |
1 | 1 | !F1 |
INIT[19] | INIT[18] | P |
---|---|---|
0 | 0 | 0 |
0 | 1 | Y |
1 | X | 1 |
The equation of S is given by:
S=Y^CC
16.3.1.22 CC_CONFIG
(Ask a Question)The CC_CONFIG macro is responsible for generating the Carry bit for each ARI1_CC cell in the cluster.

Input | Output |
---|---|
CI, P, UB | CO, CC |
CI and CO are the carry-in and carry-out, respectively, to the cell. The intermediate carry-bits are given by CC[11:0]. The functionality of the CC_CONFIG is basically evaluating CC using
CC[n] = !Px!UB+PxCC[n-1]
where CC[-1] is CI and CC[12] is CO.
Inside every cluster, there are 12 ARI1_CC cells and only one CC_CONFIG cell. The CC_CONFIG takes as input the P and UB outputs of each ARI1_CC cell in the cluster and generated the CC (carry-out bit), which is then fed to the next ARI1_CC cell in the cluster as the carry-in.
[Required-Cleanup]:16.3.1.23 FCEND_BUFF
(Ask a Question)Buffer, driven by the FCO pin of the last macro in the Carry-Chain.
Input | Output |
---|---|
A | Y |
A | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.23.1 FCINT_BUFF
(Ask a Question)
Input |
Output |
---|---|
A |
Y |
A | Y |
---|---|
0 | 0 |
1 | 1 |
16.3.1.24 RCOSC_50MHZ
(Ask a Question)The RCOSC_50MHZ oscillator is an RC oscillator that provides a free-running clock of 50 MHz at CLKOUT.
16.3.1.26 SYSRESET
(Ask a Question)It is a special-purpose macro. The Output POWER_ON_RESET_N goes low at power-up and when DEVRST_N goes low.
Input | Output |
---|---|
DEVRST_N | POWER_ON_RESET_N |
DEVRST_N | POWER_ON_RESET_N |
---|---|
0 | 0 |
1 | 1 |
16.3.1.27 SYSCTRL_RESET_STATUS
(Ask a Question)- At simulation time t = 0, set
RESET_STATUS
= 0. - 1.46 µs after observing
POWER_ON_RESET_N
= 1, setRESET_STATUS
= 1 to indicate that the system controller has entered suspend mode.
16.3.1.28 DFN1
(Ask a Question)Input | Output |
---|---|
D, CLK | Q |
CLK | D | Qn+1 |
---|---|---|
not Rising | X | Qn |
— | D | D |
16.3.1.29 DFN1C0
(Ask a Question)Input | Output |
---|---|
D, CLK, CLR | Q |
CLR | CLK | D | Qn+1 |
---|---|---|---|
0 | X | X | 0 |
1 | not Rising | X | Qn |
1 | — | D | D |
16.3.1.30 DFN1E1
(Ask a Question)Input | Output |
---|---|
D, E, CLK | Q |
E | CLK | D | Qn+1 |
---|---|---|---|
0 | X | X | Qn |
1 | not Rising | X | Qn |
1 | — | D | D |
16.3.1.31 DFN1E1C0
(Ask a Question)Input | Output |
---|---|
CLR, D, E, CLK | Q |
CLR | E | CLK | D | Qn+1 |
---|---|---|---|---|
0 | X | X | X | 0 |
1 | 0 | X | X | Qn |
1 | 1 | not Rising | X | Qn |
1 | 1 | — | D | D |
16.3.1.32 DFN1E1P0
(Ask a Question)D-Type Flip-Flop with active-high Enable and active-low Preset.
Input | Output |
---|---|
D, E, PRE, CLK | Q |
PRE | E | CLK | D | Qn+1 |
---|---|---|---|---|
0 | X | X | X | 1 |
1 | 0 | X | X | Qn |
1 | 1 | not Rising | X | Qn |
1 | 1 | ↑ | D | D |
16.3.1.33 DFN1P0
(Ask a Question)Input | Output |
---|---|
D, PRE, CLK | Q |
PRE | CLK | D | Qn+1 |
---|---|---|---|
0 | X | X | 1 |
1 | not Rising | X | Qn |
1 | — | D | D |