10.1.3.3 set_io

The set_io command assigns an I/O technology, places, or locks the I/O at a given pin location. Two I/O types are available for PolarFire:
  • GPIO
  • HSIO
Each I/O type supports different I/O standards.
Table 10-10. set_io Standards
I/O TypesSupported I/O Standards
HSIOLVCMOS12, LVCMOS15, LVCMOS18, SSTL18I, SSTL18II, HSUL18I, HSUL18II, SSTL15I, SSTL15II, HSTL15I, HSTL15II, SSTL135I, SSTL135II, HSTL135I, HSTL135II, HSTL12I, HSTL12II, HSUL12I, SLVSE15, POD12I, POD12II, SLVS18, HCSL18, LVDS18, RSDS18, MINILVDS18, SUBLVDS18, PPDS18, LCMDS18, SHIELD18, SHIELD15, SHIELD135, SHIELD12
GPIOLVTTL, LVCMOS33, PCI, LVCMOS12, LVCMOS15, LVCMOS18, LVCMOS25, SSTL25I, SSTL25II, SSTL18I, SSTL18II, HSUL18I, HSUL18II, SSTL15I, SSTL15II, HSTL15I, HSTL15II, SLVS33, HCSL33, HCSL25, MIPI25, MIPIE25, LVPECL33, LVPECL25, LVPECLE33, LVDS18G, LVDS25, LVDS33, RSDS25, RSDS33, MINILVDS25, MINILVDS33, SUBLVDS25, SUBLVDS33, PPDS25, PPDS33, SLVSE15, MLVDSE25, BUSLVDSE25, LCMDS33, LCMDS25, SHIELD33, SHIELD25, SHIELD18, SHIELD15, SHIELD12
Note: LCMDS18 IOSTD is not supported for MPF300XT devices.

The following is the syntax for this command:

set_io -port_name <port_name> \
       [-pin_name <package_pin>] \
       [-fixed <true|false>] \
       [-io_std <io_std_values>] \
       [-OUT_LOAD <value>] \
       [-RES_PULL <value>] \ 
       [-LOCK_DOWN <value>] \
       [-CLAMP_DIODE <value>] \
       [-SCHMITT_TRIGGER <value>] \
       [-SLEW <value>] \
       [-VCM_RANGE <value>] \ 
       [-ODT <value>] \
       [-ODT_VALUE] \
       [-OUT_DRIVE <value>] \ 
       [-IMPEDANCE <value>] \
       [-SOURCE_TERM <value>] \ 
       [-IN_DELAY <value>] \
       [-OUT_DELAY <value>]

Arguments

-port_name <port_name>
Specifies the port name of the I/O macro.
-pin_name <package_pin>
Specifies the package pin name(s) on which to place the I/O.
-io_std <value>

Sets the I/O standard for this macro. If the voltage standard used with the I/O is not compatible with other I/Os in the I/O bank, assigning an I/O standard to a port invalidates its location and automatically unassigns the I/O.

The following table lists the supported values for -io_std and their corresponding I/O standards. Some I/O standards support only single I/O or differential I/Os, while others support both single and differential I/Os.

Table 10-11. -io_std Values and Corresponding I/O Standards
-io_std ValueI/O Standard
SingleDifferential
LVTTLYESNO
LVCMOS33YESNO
LVCMOS25YESNO
LVCMOS18YESNO
LVCMOS15YESNO
LVCMOS12YESNO
PCIYESNO
POD12IYESYES
POD12IIYESYES
PPDS33NOYES
PPDS25NOYES
PPDS18NOYES
SLVS33NOYES
SLVS25NOYES
SLVS18NOYES
HCSL33NOYES
HCSL25NOYES
HCSL18NOYES
SLVSE15NOYES
BUSLVDSENOYES
BUSLVDSE25NOYES
MLVDSENOYES
MLVDSE25NOYES
LVDSNOYES
LVDS25NOYES
LVDS18NOYES
LVDS18GNOYES
BUSLVDSNOYES
BUSLVDSE25NOYES
MLVDSNOYES
MIPI25NOYES
MIPIE25NOYES
MIPIE33NOYES
MINILVDSNOYES
MINILVDS33NOYES
MINILVDS25NOYES
MINILVDS18NOYES
RSDSNOYES
RSDS33NOYES
RSDS25NOYES
RSDS18NOYES
LVPECL (only for inputs)NOYES
LVPECL33NOYES
LVPECLE33NOYES
HSTL15IYESYES
HSTL15IIYESYES
HSTL135IYESYES
HSTL135IIYESYES
HSTLI2IYESYES
HSTL12IIYESYES
SSTL18IYESYES
SSTL18IIYESNO
SSTL15IYESYES
SSTL15IIYESNO
SSTL135IYESYES
SSTL135IIYESYES
SSTL25IYESYES
SSTL25IIYESYES
HSUL18IYESYES
HSUL18IIYESYES
HSUL12IYESYES
HSUL12IIYESYES
SUBLVDS33NOYES
SUBLVDS25NOYES
SUBLVDS18NOYES
LCMDS33NOYES
LCMDS25NOYES
LCMDS18NOYES
SHIELD33YESNO
SHIELD25YESNO
SHIELD18YESNO
SHIELD15YESNO
SHIELD135YESNO
SHIELD12YESNO
-fixed <value>

Specifies whether the location of this port is fixed (that is, locked). Locked ports are not moved during layout. The default value is true. You can enter one of the following values.

Table 10-12. -fixed Values
ValueDescription
TrueThe location of this port is locked.
FalseThe location of this port is unlocked.
-OUT_LOAD <value>

Sets the output load (in pF) of output signals. The default is 5 pF.

Direction: Output

-RES_PULL <value>

Allows you to include a weak resistor for either pull-up or pull-down of the input and output buffers. Not all I/O standards have a selectable resistor pull option.

The following table lists the acceptable values for the -RES_PULL attribute for the input buffer.

Table 10-13. -RES_PULL Values (Input Buffer)
I/O StandardsValueDescription
Single I/Os: LVTTL, LVCMOS33, LVCMOS25, LVCMOS18, LVCMOS15, LVCMOS12, PCIUpIncludes a weak resistor for pull-up of the input buffer.
DownIncludes a weak resistor for pull-down of the input buffer.
HoldHolds the last value.
NoneDoes not include a weak resistor.
Differential I/Os: PPDS25, PPDS33, HCSL33, HCSL25, BUSLVDSE25, LVDS33, LVDS25, LVDS18G, MINILVDS33, MINILVDS25, RSDS33, RSDS25, LVPECL33, SUBLVDS33, SUBLVDS25, LCMDS33, LCMDS25UpIncludes a weak resistor for pull-up of the input buffer.
DownIncludes a weak resistor for pull-down of the input buffer.

For I/O standards in the preceding table, the default is Up. For all other I/O standards, the value is None.

The following table lists the acceptable values for the -RES_PULL attribute for the output buffer.

Table 10-14. -RES_PULL Values (Output Buffer)
I/O StandardsValueDescription
Single I/Os: LVTTL, LVCMOS33, LVCMOS25, LVCMOS18, LVCMOS15, LVCMOS12, PCIUpIncludes a weak resistor for pull-up of the output buffer.
DownIncludes a weak resistor for pull-down of the output buffer.
NoneDoes not include a weak resistor.
Note:
  • For all I/O standards, the default value for output buffer is None.
  • For output differential I/Os, res_pull is not supported.

Direction: Inout

-LOCK_DOWN <value>

Security feature that locks down the I/Os, if tampering is detected. Values are ON and OFF. The default is OFF.

Direction: Inout

-CLAMP_DIODE <value>

Specifies whether to add a power clamp diode to the I/O buffer. This attribute option is available to all I/O buffers with I/O technology set to LVTTL. A clamp diode provides circuit protection from voltage spikes, surges, electrostatic discharge, and other overvoltage conditions.

Values are OFF and ON.

The following table lists the values for GPIO standards. For HSIO standards, the value is always ON.

Table 10-15. -CLAMP_DIODE Values
I/O StandardsValues
LVCMOS12, LVCMOS15, LVCMOS18, SSTL18I, SSTL18II, SSTL15I, SSTL15II, HSTL15I, HSTL15II, LVTTL, LVCMOS33, LVCMOS25, SSTL25I, SSTL25II, SLVS25, HCSL25, LVDS25, RSDS25, MINILVDS25, SUBLVDS25, PPDS25, LCMDS25OFF, ON. The default is ON.
MIPI25, LVDS18GOFF, ON. The default is OFF.
HSUL18I, HSUL18II, SLVSE15, PCI, SLVS25, SLVS33, HCSL33, HCSL25, MIPIE33, MIPIE25, LVPECL33, LVPECL25, LVPECLE33, LVDS25, LVDS33, RSDS25, RSDS33, MINILVDS25, MINILVDS33, SUBLVDS25, SUBLVDS33, PPDS25, PPDS33, MLVDSE25, BUSLVDSE25, LCMDS25, LCMDS33ON

Direction: Inout

Note: For input LVDS18G, the only supported value for Clamp Diode is OFF.
-SCHMITT_TRIGGER <value>

Specifies whether this I/O has an input Schmitt Trigger. The Schmitt Trigger introduces hysteresis on the I/O input. This allows very slow moving or noisy input signals to be used with the part without false or multiple I/O transitions taking place in the I/O.

For the following I/O standards, the values are OFF and ON. The default is OFF.

Table 10-16. -SCHMITT_TRIGGER Values
I/O StandardsValues
GPIO
LVCMOS25, LVCMOS33, LVTTL, PCIOFF, ON
HSIO
LVCMOS18, LVCMOS15OFF, ON

For all other I/O standards, the value is OFF.

Direction: Input

-SLEW <value>

Sets the output slew rate. Slew control affects only the falling edges for some families. Slew control affects both rising and falling edges. Not all I/O standards have a selectable slew. Whether you can use the slew attribute depends on which I/O standard you have specified for this command.

The following I/O standards have values OFF and ON. The default is OFF.

Table 10-17. -SLEW Values
I/O StandardsValues
LVCMOS25, LVCMOS33, LVTTL, PCIOFF, ON

For all other I/O standards, the value is OFF.

Direction: Output

-VCM_RANGE <value>

Sets the VCM input range.

The following table lists the supported values and I/O standards.

Table 10-18. -VCM_RANGE Values
I/O StandardsValues
GPIO
HSTL15I, HSTL15II, HSUL18I, HSUL18II, SSTL15I, SSTL15II, SSTL18I, SSTL18II, SSTL25I, SSTL25IIMID
HCSL33, HCSL25, LVDS18G, LVDS33, LVDS25, LVPECL33, LVPECLE33, MINILVDS33, MINILVDS25, MIPI25, MIPIE25, MLVDSE25, PPDS33, PPDS25, RSDS33, RSDS25, SLVS33, SLVS25, SLVSE15, BUSLVDSE25, SUBLVDS33, SUBLVDS25
Note:

While assigning VCM input range for true differential I/Os in the same bank, a mix of MID and LOW values cannot be assigned for the I/Os. You can assign only MID or only LOW values for all differential I/Os in the same bank.

If a mixture of VCM input ranges is needed for true differential inputs within the same GPIO bank, to optimize or tune the interface performance in hardware, the I/O attribute can be set using the Post Layout I/O Editing flow in the Libero Design Flow User Guide, and the edit_io command. For more information, see edit_io. In that scenario, the internal 100 Ohm on-die differential termination resistor accuracy percentage tolerance will follow the maximum percentage tolerance of the two ranges per the device datasheet specifications.

MID, LOW. The default is MID.
LCMDS33, LCMDS25LOW
HSIO
HSTL12I, HSTL12II, HSTL135I, HSTL135II, HSTL15I, HSTL15II, HSUL12I, HSUL18I, HSUL18II, LVSTL11I, LVSTL11II, POD12I, POD12II, SSTL135I, SSTL135II, SSTL15I, SSTL15II, SSTL18I, SSTL18IIMID
SLVSE15, LVDS18, HCSL18, MINILVDS18, PPDS18, RSDS18, SLVS18, SUBLVDS18MID, LOW. The default is MID.
LCMDS18LOW

Direction: Input

-ODT <value>

On-die Termination (ODT) is the technology where the termination resistor for impedance matching in transmission lines is located inside a semiconductor chip instead of on a printed circuit board.

In case of LVDS fail-safe mode, use the DYNAMIC value for ODT.

Values are OFF and ON.

The following table lists acceptable values.

Table 10-19. -ODT Values
I/O StandardsValues
LVCMOS12, LVCMOS15, LVCMOS18, LVCMOS25OFF, ON. The default is OFF.
HSUL18I, HSUL18II

OFF, ON, DYNAMIC. The default is OFF.

SSTL15I, SSTL15II, SSTL18I, SSTL18II, HSUL12I, LVSTL11I, LVSTL11II, POD12I, POD12II, SSTL135I, SSTL135II, HSTL15I, HSTL15II, LVDS18G, LVDS33, LVDS25, LVPECL33, LVPECLE33, LVPECL25, MINILVDS33, MINILVDS25, RSDS33, RSDS25, SUBLVDS33, SUBLVDS25, HSTL12I, HSTL12II, HSTL135I, HSTL135II, LCMDS33, LCMDS25OFF, ON, DYNAMIC. The default is ON.

Direction: Input

-ODT_VALUE

Sets the ODT value in Ohms.

Values vary depending on the I/O standard. The following table lists acceptable values.

Table 10-20. -ODT_VALUE Values
I/O StandardsValues
LVCMOS12, LVCMOS15, LVCMOS18120, 240. The default is 120.
LVCMOS25120
HSUL12I60, 120, 240. The default is 120.
SSTL15I, SSTL15II20, 30, 40, 60, 120. The default is 30.
SSTL135I, SSTL135II20, 30, 40, 60, 120. The default is 40.
SSTL18I, SSTL18II50, 75, 150. The default is 50.
POD12I, POD12II34, 40, 48, 60, 80, 120, 240. The default is 60.
LVDS18G, LVDS33, LVDS25, LVPECL33, LVPECL25, MINILVDS33, MINILVDS25, RSDS33, RSDS25, SLVSE15, SUBLVDS33, SUBLVDS25, LCMDS33, LCMDS25100
HSTL15I, HSTL15II, HSUL18I, HSUL18II, HSTL12I, HSTL12II, HSTL135I, HSTL135II50

Direction: Inout

-OUT_DRIVE <value>

Sets the strength of the output buffer to 1.5, 2, 3.5, 4, 6, 8, 10, 12, 16, or 20 in mA, weakest to strongest. The list of I/O standards for which you can change the output drive and the list of values you can assign for each I/O standard is family-specific. Not all I/O standards have a selectable output drive strength.

Each I/O standard has a different range of legal output drive strength values. The values you can choose depend on which I/O standard you specified for this command. The following table lists the acceptable values.

Table 10-21. -OUT_DRIVE Values
I/O StandardValues
GPIO
LVCMOS122, 4, 6, 8. Default is 8.
LVCMOS152, 4, 6, 8, 10. Default is 8.
LVCMOS182, 4, 6, 8, 10, 12. Default is 8.
LVCMOS252, 4, 6, 8, 12, 16. Default is 8.
LVCMOS33, LVTTL2, 4, 8, 12, 16, 20. Default is 8.
LVDS18G, LVDS25, LVDS33, MINILVDS25, MINILVDS33, LCMDS33, LCMDS253, 3.5, 4, 6. Default is 6.
PPDS25, PPDS33, RSDS25, RSDS331.5, 2, 3. Default is 3.
SUBLVDS25, SUBLVDS331, 1.5, 2. Default is 2.
BUSLVDSE25, MLVDSE25, LVPECLE3316
MIPIE25, SLVSE158
PCI20
HSIO
LVCMOS12, LVCMOS152, 4, 6, 8, 10. Default is 8.
LVCMOS182, 4, 6, 8, 10, 12. Default is 8.
SLVSE158

Direction: Output

-IMPEDANCE

Sets the impedance value in Ohms.

Values vary depending on the I/O standards.

Direction: Output

-SOURCE_TERM

Near-end termination for a differential output I/O. The following table lists the acceptable values.

Table 10-22. -SOURCE_TERM Values
I/O StandardsValues
LVDS18G, LVDS25, LVDS33, MINILVDS25, MINILVDS33, LCMDS33, LCMDS25, PPDS25, PPDS33, RSDS25, RSDS33, SUBLVDS25, SUBLVDS331OFF, 100. The default is OFF.

Direction: Output

-IN_DELAY

Sets the static input delay.

Input delay applies to all I/O standards. The values are OFF and 0–127, 128, 130, 132,...254. The default value is OFF.

Direction: Input

Note:
  • This attribute does not appear in the I/O attributes and cannot be used in the PDC for some I/Os with dynamic delays, such as DDR, LPDDR, QDR memory interfaces and I/O CDR interfaces.
  • For the dynamically delayed I/O interfaces that also support setting a static delay value, this attribute will be listed as OFF if a static delay has not been added. You can still adjust the dynamic delays during normal operation, even if the static delay is listed as OFF.
-OUT_DELAY

Sets the static output delay.

Output delay applies to all I/O standards. The values are OFF and 0–127. The default value is OFF.

Direction: Output

Note:
  • This attribute does not appear in the I/O attributes and cannot be used in the PDC for some I/Os with dynamic delays, such as DDR, LPDDR, QDR memory interfaces and I/O CDR interfaces.
  • In case of LVDS fail-safe mode, you can use the following PDC commands:
    • Weak pull-up/pull-down resistor for differential inputs.
      set_io -RES_PULL <value>
    • Dynamic ODT access per I/O.
      set_io -ODT DYNAMIC
  • For the dynamically delayed I/O interfaces that also support setting a static delay value, this attribute will be listed as OFF if a static delay has not been added. You can still adjust the dynamic delays during normal operation, even if the static delay is listed as OFF.

Examples

set_io -port_name IO_in\[2\] 
-io_std LVCMOS25 \ 
-fixed true\

I/O Directions Not Supported

The following table lists the I/O directions that are not supported for I/O standards.

Table 10-23. I/O Directions That are Not Supported (set_io)
I/O DirectionIO_STD Value
InputSLVSE15, MLVDSE25, BUSLVDSE25, MIPIE33, LVPECLE33, SHIELD33, SHIELD25, SHIELD18, SHIELD15, SHIELD135, SHIELD12
OutputSLVS33, SLVS25, HCSL33, HCSL25, LVPECL33, LVPECL25, MIPI25, LVDS18, RSDS18, MINILVDS18, SUBLVDS18, PPDS18, SLVS18, HCSL18, LCMDS18
TribuffSLVS33, SLVS25, HCSL33, HCSL25, LVPECL33, LVPECL25, MIPI25, LVDS18, RSDS18, MINILVDS18, SUBLVDS18, PPDS18, SLVS18, HCSL18, LVDS18G, LVDS25, LVDS33, RSDS25, RSDS33, MINILVDS25, MINILVDS33, SUBLVDS25, SUBLVDS33, PPDS25, PPDS33, LCMDS25, LCMDS33, LCMDS18
InoutLVDS18G, LVDS33, LVDS18, LVDS25, RSDS18, RSDS33, RSDS25, MINILVDS18, MINILVDS33, MINILVDS25, SUBLVDS18, SUBLVDS33, SUBLVDS25, PPDS18, PPDS33, PPDS25, SLVS33, SLVS25, HCSL33, HCSL25, LVPECL33, LVPECL25, MIPI25, MIPIE25, SLVS18, HCSL18, SHIELD33, SHIELD25, SHIELD18, SHIELD15, SHIELD135, SHIELD12, LCMDS25, LCMDS33, LCMDS18