20.2.1 Installing the PolarFire SoC MSS Configurator
(Ask a Question)The PolarFire SoC MSS Configurator bundled with Libero is available at the following location in the Libero installation section:
-
Windows: <$Installation_Directory>\Microsemi\Libero_SoC_vX.X\Designer\bin64\pfsoc_mss.exe -
Linux: <$Installation_Directory>\Microsemi\Libero_SoC_vX.X\bin64\pfsoc_mss
The PolarFire SoC MSS Configurator can also be installed as a stand-alone application.
For more information about how to install Libero, see Libero SoC v12.0 and later .
20.2.1.1 Input and Output Files
(Ask a Question)The following sections describe the PolarFire SoC MSS Configurator input and output files.
20.2.1.1.1 Output Files
(Ask a Question)The PolarFire SoC MSS Configurator generates the output file formats as shown in the following figure.
-
XML Configuration File: Contains the MSS memory map, clock, DDR memory controller, and peripheral configuration. The XML file is used to generate hardware files required for building the firmware project.
- CXZ File: Encapsulates the hardware design of the MSS block and can be imported into Libero SoC project.

20.2.1.1.2 Input files
(Ask a Question)The PolarFire SoC MSS Configurator can be invoked without any input files. A configuration file
(.cfg) from an earlier MSS configurator session can be optionally provided
to the PolarFire SoC MSS Configurator.
.cfg file and a report file
can also be generated from the PolarFire SoC MSS Configurator.