3.6.2 Constraints Manual
(Ask a Question)Learn more about the constraints available for SmartHLS.
3.6.2.1 Constraints Manual
(Ask a Question)SmartHLS™ accepts user-provided constraints that impact the automatically generated hardware. These constraints can be specified using the SmartHLS IDEand are stored in the Tcl configuration file config.tcl located in your project directory. This section provides information about the constraints available for SmartHLS. The main constraints available from the SmartHLS IDE are:
- Set target clock period: CLOCK_PERIOD
- Print the HDL output to a single output file: SINGLE_HDL_OUTPUT_FILE
- Set custom config file: set_custom_config_file
- Set test bench file: set_custom_test_bench_file
- Set test bench module: set_custom_test_bench_module
- Set operation latency: set_operation_latency
- Set FPGA family and device: set_project
- Set resource constraint: set_resource_constraint
- Set FPGA synthesis top-level module: set_synthesis_top_module
- Set FPGA synthesis top-level file: set_synthesis_top_module_file
A few debugging constraints are available from the SmartHLS IDE:
- Stalling input/output FIFOs in CoSimulation: COSIM<INPUT|OUTPUT>_FIFO_STALL_PROB
- Keep signals with no fanout: KEEP_SIGNALS_WITH_NO_FANOUT
- Insert simulation assertions (for debugging): VSIM_ASSERT
3.6.2.2 Commonly Used Constraints
(Ask a Question)3.6.2.2.1 CLOCK_PERIOD
(Ask a Question)This is a widely used constraint that allows the user to set the target clock period for a design. The clock period is specified in nanoseconds.
It has a significant impact on scheduling: the scheduler will schedule operators into clock cycles using delay estimates for each operator, such that the specified clock period is honored. In other words, operators will be chained together combinationally to the extent allowed by the value of the CLOCK_PERIOD parameter.
SmartHLS™ has a default CLOCK_PERIOD value for each device family that is supported (see table in SmartHLS Constraints).
- Category
- HLS Constraints
- Value Type
- Decimal or integer; represents a value in nanoseconds
- Valid Values
- Positive decimal or positive integer
- Default Value
- Depends on the target device
- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter CLOCK_PERIOD 15
3.6.2.2.2 SINGLE_HDL_OUTPUT_FILE
(Ask a Question)When set to 1, this Tcl parameter constrains
SmartHLS-generated Verilog RTL and VHDL wrapper modules to a
single Verilog file (<Project Name>.v) and a single VHDL file
(<Project Name>.vhd) respectively. By default, each Verilog
top-level module (and its child modules) is printed to a separate output file
(<Project Name>_<Top-Level Name>.v), and each VHDL
wrapper module of a top-level is printed to a separate VHDL file (<Project
Name>_<Top-Level Name>.vhd).
- Category
- HLS Constraints
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
SINGLE_HDL_OUTPUT_FILE 0- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter SINGLE_HDL_OUTPUT_FILE 1
3.6.2.2.3 set_custom_config_file
(Ask a Question)If you want to add advanced SmartHLS™ Tcl constraints that are not listed in the SmartHLS IDE constraints dialog you need to use a custom config file. Be careful not to modify the config.tcl constraints file directly, since config.tcl will be overwritten whenever you make changes in the SmartHLSIDE constraints dialog.
- Open the SmartHLS Constraints Menu.
- Select
Set custom config filefrom the dropdown and enter the Constraint Value as "custom_config.tcl". - Click Add:

Now click OK:

Now in the Project Explorer, right click and select New > File:

Enter the name of "custom_config.tcl". This should match the file name entered in the Set HLS Constraints previously. Click Finish:

3.6.2.2.4 set_custom_test_bench_file
(Ask a Question)This Tcl command is to specify the user-provided custom testbench file that defines the
custom testbench module, which is set via set_custom_test_bench_module.
This is not needed for SW/HW co-simulation.
- Category
- Simulation
- Value Type
- String
- Dependencies
set_custom_test_bench_module "user_tb"- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_custom_test_bench_file user_tb.v
3.6.2.2.5 set_custom_test_bench_module
(Ask a Question)This Tcl command is to specify the name of the user-provided testbench module to be using for RTL simulation. The testbench file must also be specified withset_custom_test_bench_file .
- Category
- Simulation
- Value Type
- String
- Dependencies
set_custom_test_bench_file user_tb.v- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_custom_test_bench_module "user_tb"
3.6.2.2.6 set_operation_latency
(Ask a Question)This Tcl command sets the latency of a given operation.Latency refers to the number of clock cycles required to complete the computation; an operation with latency one requires one cycle, while zero-latency operations are completely combinational, meaning multiple such operations can be chained together in a single clock cycle. This command is used to schedule each type operation to take the specified number of cycles.
This Tcl command should only be used by advanced SmartHLS™ users.
- Category
- HLS Constraints
- Value Type
set_operation_latency <operation> <constraint>, in which<operation>is a string and<constraint>is an integer- Valid Values
- See Default and Examples.
- Default Values
fp_add_64 12 fp_add_32 11 fp_subtract_64 12 fp_subtract_32 11 fp_multiply_64 8 fp_multiply_32 5 fp_divide_32 33 fp_divide_64 61 fp_truncate_64 5 fp_extend_32 4 fp_signed_comp_o 3 fp_signed_comp_u 3 fp_sitofp_32_32 4 fp_sitofp_32_64 5 fp_sitofp_64_32 5 fp_sitofp_64_64 5 fp_uitofp_32_32 4 fp_uitofp_32_64 4 fp_uitofp_64_32 5 fp_uitofp_64_64 4 fp_fptosi_32_32 4 fp_fptosi_32_64 5 fp_fptosi_64_32 4 fp_fptosi_64_64 5 fp_fptoui_32_32 4 fp_fptoui_32_64 5 fp_fptoui_64_32 4 fp_fptoui_64_64 5 reg 2 external_memory_port 1
- Location Where Default is Specified
devices/Microchip.tcland
devices/set_operation_latency.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
# set memory operations to take 3 cycles
3.6.2.2.7 set_project
(Ask a Question)This parameter sets the default target project, or device, used. Changing the project also updates the associated family and board parameters.
This parameter has 3 arguments:
- FPGA Family (e.g. PolarFire®).
- FPGA Device: This can either be the board name (e.g. MPF300), or the device number (e.g. MPF300TS-1FCG1152I).
- Flow:
hw_only,Icicle_SoCorMiV_SoC.hw_only: SmartHLS only generates an IP core.Icicle_SoC: SmartHLS SoC commands generate a reference design targeting the PolarFire® SoC Icicle kit devices.MiV_SoC: SmartHLS SoC commands generate a MiV RV32 reference design targeting the PolarFire® Video Kit board.
- Category
- Board and Device Specification
- Value Type
- String
- Valid Values
- See Examples
- Default Value
PolarFire MPF300 hw_only- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_project PolarFire MPF300 hw_only
3.6.2.2.8 set_resource_constraint
(Ask a Question)This Tcl command constrains the resource allocated by SmartHLS™. For instance, to only have a single divider in the entire circuit, user can specify: set_resource_constraint divide 1. This makes SmartHLS instantiate a maximum of 1 divider in the circuit, and if there are multiple division operations required, they will share the same divider.
- signed_divide_8
- signed_divide_16
- signed_divide_32
- signed_divide_64
- unsigned_divide_8
- unsigned_divide_16
- unsigned_divide_32
- unsigned_divide_64
It can also be used to constrain the number of memory ports. To make all memories single-ported: set_resource_constraint memory_port 1 For memory ports, only 1 and 2 are valid values, as FPGA RAMs have up to 2 ports.
This Tcl command should only be used by advanced SmartHLS users.
- Category
- HLS Constraints
- Value Type
set_resource_constraint <operation> <constraint>, in which<operation>is a string and<constraint>is an integer- Valid Values
- See Default and ExamplesImportant: Operator name should match the device family operation database file: boards/PolarFire/PolarFire.tcl
- Default Values
memory_port 2 divide 1 modulus 1 fp_add 1 fp_subtract 1 fp_multiply 1 fp_divide 1 fp_truncate 1 fp_extend 1 fp_fptosi 1 fp_sitofp 1- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_resource_constraint signed_divide_16 3
The multiply splitting feature (see ENABLE_MULTIPLY_SPLITTING) does not support multiplier
sharing. Therefore, if a user specifies set_resource_constraint multiply
X, multiplication splitting will be disabled, regardless of the value
set to ENABLE_MULTIPLY_SPLITTING. In such cases, SmartHLS will issue a warning message: Warning:
Detected set_resource_constraint setting for integer multiplier. However,
multiplier sharing is incompatible with the multiply splitting feature.
Disabling multiply splitting feature and the normal multiplier modules will be
used.
In this case, the latency of all multiplication operations will be determined by the
value set in the set_operation_latency multiply X command. If this
command is not used, latency will default to 2.
3.6.2.2.9 set_synthesis_top_module
(Ask a Question)This Tcl command specifies the name of the Verilog module that will be set as the top-level module when creating a Libero project for synthesis, place and route. By default, the top-level function (see Specifying the Top-level Function) is set as the top-level module for the Libero project, however user may want to provide wrapper HDL module that instantiates the SmartHLS-generate top-level module. In this case, this Tcl command can be used to give the name of the wrapper module.
- Category
- Libero
- Value Type
- String
- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_synthesis_top_module "wrapper_top"
3.6.2.2.10 set_synthesis_top_module_file
(Ask a Question)When set_synthesis_top_module is used to set a different wrapper module as the top-level for synthesis, place & route, use this command to specify the file that defines the wrapper module.
- Category
- Libero
- Value Type
- String
- Dependencies
set_synthesis_top_module "wrapper_top"- Applicable Flows
- All devices and flows
- Test Status
- Actively in use
- Examples
set_synthesis_top_module_file custom_synthesis_top.v
3.6.2.3 Debugging Constraints
(Ask a Question)3.6.2.3.1 COSIM<INPUT|OUTPUT>_FIFO_STALL_PROB
(Ask a Question)The COSIM_INPUT_FIFO_STALL_PROB and COSIM_OUTPUT_FIFO_STALL_PROB parameters can be used to exercise halting data injecting to input FIFO or backpressuring the output FIFO during Simulate HLS Hardware (SW/HW Co-Simulation). When the parameter is set to a value between 1 and 99, representing the probablity to halt input FIFO or backpressure output FIFO, the SmartHLS-generated CoSimulation testbench will randomly halt the data injectiion to input FIFO or backpressure output FIFO, which will then cause the SmartHLS-generated circuit to stall during simulation.
- Category
- HLS Constraint
- Value Type
- Integer
- Valid Values
- 0-100
- Default Value
- 0: disabled
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in use
- Examples
set_parameter COSIM_INPUT_FIFO_STALL_PROB 50
3.6.2.3.2 KEEP_SIGNALS_WITH_NO_FANOUT
(Ask a Question)If this parameter is enabled, all signals will be printed to the output Verilog file, even if they don't drive any outputs.
- Category
- HLS Constraint
- Value Type
- Integer
- Valid Values
- 0, 1
- Default Value
- 0
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in use
- Examples
set_parameter KEEP_SIGNALS_WITH_NO_FANOUT 1
3.6.2.3.3 VSIM_ASSERT
(Ask a Question)When set to 1, this constraint causes assertions to be inserted in the Verilog produced by SmartHLS™. This is useful for debugging the circuit to see where invalid values (X's) are being assigned.
- Category
- Simulation
- Value Type
- Integer
- Valid Values
- 0, 1
- Default Value
- 0
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in use
- Examples
set_parameter VSIM_ASSERT 1
3.6.2.4 Advanced Constraints
(Ask a Question)3.6.2.4.1 IFCONV_PREDICATE_LOADS
(Ask a Question)This constraint sets whether load instructions should be predicated during if-conversion. By default, it is set to 1 to predicate load instructions to avoid resource contention between mutually exclusive loads. If there is no resource contention between mutually exclusive loads, it can set to 0 avoid inserting predication logic.
- Category
- HLS Constraints
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 1
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in use
- Examples
set_parameter IFCONV_PREDICATE_LOADS 1
3.6.2.4.2 LATENCY_REDUCTION
(Ask a Question)The LATENCY_REDUCTION settings control the SmartHLS's expression balancing optimization, of which the objective is to reduce the circuit latency. Below are the related settings:
| Parameter Name | Default Value | Description |
|---|---|---|
| LATENCY_REDUCTION | 1 | The main switch that enables or disables expression balancing. Setting to 0 disables all expression balancing optimizations. |
| LATENCY_REDUCTION_ALLOW_FP_REORDERING | 0 | By default, expression balancing does not re-order floating-point operations to prevent loss
of precisions. Setting to 1 allows to re-order floating-point operations if the circuit latency can be reduced. Because the floating point operations may lose
their commutativity and associativity with finite precision, this optimization may
result in the failure of the co-simulation. CAUTION: This is an unsafe optimization.
Users should only enable this option on error tolerant designs. |
| LATENCY_REDUCTION_REDUCE_FP_CONVERSIONS | 0 | Setting to 1 will allow SmartHLS™ to cancel out back-and-forth conversion between floating-point and integer, with potential variations in numerical values. For example, the following conversions can be cancelled when this setting is 1.
Level of accuracy loss caused by this optimization is run-time value dependent.
Therefore, carefully examine the potential value sets of the associated operations
as well as your design tolerance before enabling this option. CAUTION: This is an unsafe optimization.
Users should only enable this option on error tolerant designs. |
| LATENCY_REDUCTION_BALANCE_MULTI_USE_NODE | 0 | By default expression balancing does not optimize the intermediate operations that have multiple uses, to avoid potential increase of resource usage. Setting to 1 allows to re-order intermediate operations that have multiple uses and more latency reduction could be achieved. |
- Category
- HLS Constraints
- Value Type
- Integer
- Valid Values
- 0, 1
- Default Value
- As listed in the table above.
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter LATENCY_REDUCTION 1
3.6.2.4.3 ENABLE_AUTOMATIC_MEMORY_LATENCY_SETTING
(Ask a Question)Enable determining memory latency for reads automatically according to the target clock period and timing model of the board. Memory latency is set to 2 when the target clock period is less than the delay of memory for the target device, otherwise is set to 1. Increasing the memory latency can result in higher circuit Fmax at the expense of higher circuit latency. The auto-determined latency can be found in the Memory Usage section of SmartHLS™ report.
Setting the operation latency for a RAM will override the latency automatically calculated. See set_operation_latency for a list of valid memory port latency. The threshold for switching are listed in the table below.
| Device | Use Memory Latency of 2 when Target Period is less than (ns) |
|---|---|
| PolarFire, PolarFire SoC | 4.167 |
| IGLOO2, SmartFusion2 | 4.167 |
| PolarFire 2 | 4.167 |
ENABLE_AUTOMATIC_MEMORY_LATENCY_SETTING controls the latency for the following memory constraints. Each constraint can be used with set_operation_latency <Name> <latency> to override the auto-determined latency.
| Name | Description |
|---|---|
local_memory_port | Controls the memory latency of Local Memory used by a single function. |
shared_local_memory_port | Controls the memory latency of Shared-Local Memory shared by multiple functions. |
axi_slave_ram_memory_port | Controls the memory latency of Legacy AXI4 Slave Interface |
memory_port | Controls the memory latency of Memory Controller |
SmartHLS does not automatically determine the latency for external_memory_port as it is only for creating an interface with the RAMs outside of the circuit. However, for SmartHLS SoC Flow, external_memory_port controls the latency for the on-chip memory buffers.
- Category
- HLS Constraints
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 1
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter ENABLE_AUTOMATIC_MEMORY_LATENCY_SETTING 1
3.6.2.4.4 ENABLE_MULTIPLY_SPLITTING
(Ask a Question)- Category
- HLS constraint
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 1: enabled
- Dependencies
- None
- Test Status
- Actively in-use
- Examples
set_parameter ENABLE_MULTIPLY_SPLITTING 0
3.6.2.4.5 FORCED_MATH_BLOCK_PIPELINE_DEPTH
(Ask a Question)FORCED_MATH_BLOCK_PIPELINE_DEPTH to a non-zero value, constrained by the
target architecture.ENABLE_AUTOMATIC_MULTIPLY_MODE_SETTING and
MULTIPLY_SPLITTING_FULLY_PIPELINED removed since SmartHLS™ 2025.1, this constraint can be used to have more
precise control of Math block pipelining depth.- Category
- HLS Constraints
- Value Type
- Integer
- Valid Values
- 0, 1, 2
- Default Value
- 0
- Dependencies
- None
- Test Status
- Actively in use
- Examples
set_parameter FORCED_MATH_BLOCK_PIPELINE_DEPTH 1
3.6.2.4.6 SOC_AXI_INITIATOR
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the AXI initiator interface used by the processor in the user-defined SmartDesign system to connect to the HLS module's AXI target interface. This AXI initiator interface is used by the processor to control and transfer data to/from the HLS modules.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on using this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- String
- Default Value (Based on Icicle SoC reference design)
- AXI2AXI_TO_HLS:AXI4_MASTER
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_AXI_INITIATOR AXI2AXI_TO_HLS:AXI4_MASTER
3.6.2.4.7 SOC_AXI_TARGET
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the AXI target interface in the user-defined SmartDesign system where the HLS module's AXI initiator interface can connect to. This AXI target interface is used by the HLS modules to access shared memory (DDR) directly.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on using this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- String
- Default Value (Based on Icicle SoC reference design)
- AXI2AXI_FROM_HLS:AXI4_SLAVE
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_AXI_TARGET AXI2AXI_FROM_HLS:AXI4_SLAVE
3.6.2.4.8 SOC_BD_NAME
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the name of the SmartDesign system to integrate the HLS modules into.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- String
- Default Value (Based on Icicle SoC reference design)
- FIC_0_PERIPHERALS
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_BD_NAME FIC_0_PERIPHERALS
3.6.2.4.9 SOC_CLOCK
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the name of the clock to connect to the HLS modules. Currently, all HLS modules use the same clock.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- String
- Default Value (Based on Icicle SoC reference design)
- ACLK
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_CLOCK ACLK
3.6.2.4.10 SOC_CPU_MEM_BASE_ADDRESS
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the base address of the memory window in the shared memory space (DDR) that can be accessed by the HLS module's AXI initiator interfaces. This address is used to configure the AXI interconnect that HLS modules connect to for accessing the shared memory.
Note that the value for the parameter is specified in hexadecimal format and must be prefixed with 0x.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- Hexadecimal
- Default Value (Based on Icicle SoC reference design)
- 0x80000000
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_CPU_MEM_BASE_ADDRESS 0x80000000
3.6.2.4.11 SOC_CPU_MEM_SIZE
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the size of the shared memory (DDR) space that the HLS module's AXI initiator interfaces can access.
Note that the value for the parameter is specified in hexadecimal format and must be prefixed with 0x.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- Hexadecimal
- Default Value (Based on Icicle SoC reference design)
- 0x60000000
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_CPU_MEM_SIZE 0x60000000
3.6.2.4.12 SOC_DMA_ENGINE
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the type of DMA engine to use in the system for transferring data to/from HLS modules.
| DMA Engine | Description |
|---|---|
| HARD_DMA | Uses the DMA available in the PolarFire® SoC MSS. This implies that the CPUs to be used are the RISC-V U54 application cores in the MSS. |
| SOFT_DMA | Automatically instantiates a DMA engine on the FPGA fabric and be connected to the SmartHLS™ AXI interconnect along with the SmartHLS IP modules. Currently this option is not enabled, but will be in a future release. |
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- String
- Default Value (Based on Icicle SoC reference design)
- HARD_DMA
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- HARD_DMA is actively in-use; SOFT_DMA will be made available in a future release
- Examples
set_parameter SOC_DMA_ENGINE HARD_DMA
3.6.2.4.13 SOC_FABRIC_BASE_ADDRESS
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the base address of the CPU memory space that is reserved for all HLS modules. The control registers and on-chip memory buffers of HLS modules are allocated and mapped within this memory window. This address is also used to configure the AXI interconnect that HLS modules connect to.
Note that the value for the parameter is specified in hexadecimal format and must be prefixed with 0x.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- Hexadecimal
- Default Value (Based on Icicle SoC reference design)
- 0x70000000
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_FABRIC_BASE_ADDRESS 0x70000000
3.6.2.4.14 SOC_FABRIC_SIZE
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the size of the CPU memory space that is reserved for all HLS modules. The control registers and on-chip memory buffers of HLS modules are allocated and mapped within this memory window. This address is also used to configure the AXI interconnect that HLS modules connect to.
Note that the value for the parameter is specified in hexadecimal format and must be prefixed with 0x.
By default, 4MB of size is reserved. If this is larger than what HLS modules require, it can just be left for future use. Reserving a larger window does not mean more on-chip memory will be used.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- Hexadecimal
- Default Value (Based on Icicle SoC reference design)
- 0x400000
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_FABRIC_SIZE 0x400000
3.6.2.4.15 SOC_POLL_DELAY
(Ask a Question)This parameter controls how often an accelerator driver function polls the status register of an HLS module to check for its completion. By default, the delay is set to 0, which means the processor will continuously poll the status. However, it may be beneficial to insert a delay in polling to reduce CPU usage and power consumption. The poll delay is specified in microseconds.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- Integer; represents a value in microseconds
- Valid Values
- Non-negative integer
- Default Value (Based on Icicle SoC reference design)
- 0
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_POLL_DELAY 10
3.6.2.4.16 SOC_PROFILER_COUNTER
(Ask a Question)This parameter specifies whether or not to include a hardware counter to help profile SoC-based designs. The counter is not included by default.
For more information, see SoC Profiler.
- Category
- HLS Constraints
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 0
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_PROFILER_COUNTER 1
3.6.2.4.17 SOC_RESET
(Ask a Question)This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the name of the reset signal to connect to the HLS modules. Currently, all HLS modules use the same reset. Note that the reset polarity must be active-high.
Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.
- Category
- HLS Constraints
- Value Type
- String
- Default Value (Based on Icicle SoC reference design)
- ARESETN
- Dependencies
- None
- Applicable Flows
- SoC Flow Only
- Test Status
- Actively in-use
- Examples
set_parameter SOC_RESET ARESETN
3.6.2.4.18 STRENGTH_REDUCTION
(Ask a Question)Strength reduction is an optimization that converts multiply-by-constant into shifts and additions:
Info: StrengthReduction: Replaced 20 multipliers by constant with 20 adders in function multiply.
Info: StrengthReduction: Replaced 20 multipliers by constant with 20 adders in function multiply.
Info: StrengthReduction: Replaced 40 multipliers by constant with 40 adders in function multiply
This optimization saves DSP blocks on the FPGA but can also increase LUT usage in the design.
You can tune the number of adders allowed per multiplier with the constraint: STRENGTH_REDUCTION_ADDERS_ALLOWED_PER_MULTIPLIER
- Category
- HLS Constraints
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 1
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter STRENGTH_REDUCTION 1
3.6.2.4.19 STRENGTH_REDUCTION_ADDERS_ALLOWED_PER_MULTIPLIER
(Ask a Question)Strength reduction is an optimization that converts multiply-by-constant into shifts and additions:
Info: StrengthReduction: Replacing multiply by constant (i26 33038) with 3 adders:
- (1 << 1) + (1 << 4) + (1 << 8) + (1 << 15)
The STRENGTH_REDUCTION_ADDERS_ALLOWED_PER_MULTIPLIER constraint allows you to tune the number of adders allowed per multiplier (default is 3). Strength reduction for multiply-by-constants will not be performed if this requires more adders than allowed:
i26 16828 is composed of 4 adders:
- (1 << 2) + (1 << 6) + (1 << 7) + (1 << 8) + (1 << 14)
Skipping conversion otherwise would need too many additions.
In this example, we would need 4 adders which is more than the default of 3, meaning strength reduction will not occur and SmartHLS™ will keep the multiplier.
- Category
- HLS Constraints
- Value Type
- Integer
- Valid Values
- Non-negative integer
- Default Value
- 3
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- STRENGTH_REDUCTION must be on
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter STRENGTH_REDUCTION_ADDERS_ALLOWED_PER_MULTIPLIER 3
3.6.2.4.20 SYNTHESIS_CLOCK_PERIOD
(Ask a Question)This constraint allows the user to override the SDC clock period constraint for synthesis, P&R, and timing analysis.
By default, when this constraint is not specified, the same CLOCK_PERIOD constraint for HLS is used for the SDC clock period constraint. However, it may be useful to give a tighter SDC clock period constraint to close timing.
The clock period is specified in nanoseconds.
- Category
- HLS Constraints
- Value Type
- Decimal or integer; represents a value in nanoseconds
- Valid Values
- Positive decimal or positive integer
- Default Value
- N/A
- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter SYNTHESIS_CLOCK_PERIOD 10
3.6.2.4.21 USE_FIFO_FOR_PIPELINE_REG
(Ask a Question)In a pipeline circuit where multiple stages of the circuit are concurrently active and processing different loop iterations (or function calls), pipeline registers are used to retain and propagate a variable value from the value-producing stage to the value-use stage. The pipeline registers are essentially a chain of shift registers with additional control logic. When the chain of pipeline registers is long, it may be more resource-efficient to implement the pipeline registers as a block-RAM FIFO rather than shift registers.
When this parameter is enabled, SmartHLS™ will examine each chain of pipeline registers and use the implementation (FIFO or shift register) that is estimated to be more resource-efficient.
- Category
- HLS Constraint
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 1
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter USE_FIFO_FOR_PIPELINE_REG 1
3.6.2.4.22 COSIM_FREE_RUNNING_DATAFLOW_TOP
(Ask a Question)The COSIM_FREE_RUNNING_DATAFLOW_TOP parameter can be useful for dataflow
designs which contain conditionally-executed tasks. When the top-level module uses
dataflow, this parameter will make the top-level module free-running, i.e., its start
signal will be tied to 1. This parameter should not be enabled if an AXI Target
interface is used.
- Category
- HLS Constraint
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 0: disabled
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Alpha release
- Examples
set_parameter COSIM_FREE_RUNNING_DATAFLOW_TOP 1
3.6.2.4.23 AXI_RRESP_ALWAYS_ZERO
(Ask a Question)The AXI_RRESP_ALWAYS_ZERO parameter determines how the HLS module will respond when it receives an AXI read requests to an address that is not used within its address map; essentially an address decoding error. These gaps within the addresses map occur due to address alignments in the AXI target register interface for the function arguments.
By default the module will return AXI RRESP=2'b10 (slave error) when an address decoding error is detected. It is the responsibility of the initiator of the AXI read request to process the response accordingly and the returned value (AXI RDATA) will be undefined although most likely it will be zero.
This response code can be forced to always zero by setting AXI_RRESP_ALWAYS_ZERO = 1 constraint, essentially ignoring any address decoding error. One reason to ignore this error is to perform memory monitoring or memory readout of the entire address space of a given HLS module for debugging purposes. This can be done in SoftConsole or with debuggers like gdb as can be seen in the following image using the command x/128hw 0x50000000, which means "read 128 words and print them in hex format starting at address 0x50000000", which would be the base address of the HLS module:

- Category
- HLS Constraint
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 0: disabled
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Alpha release
- Examples
set_parameter AXI_RRESP_ALWAYS_ZERO 1
3.6.2.4.24 SYNTHESIS_FSM_ENCODING
(Ask a Question)This constraint allows users override the default finite state machine encoding chosen by the synthesis tools with the specified encoding style.
The style string value specified in this parameter will be used to generate a Synopsys synthesis attribute for each state machine register in the compiled design.
- Category
- HLS Constraints
- Value Type
- String
- Valid Values
"onehot","gray","sequential","safe","original"and combination of multiple valid values separated by comma.- Default Values
- "onehot"
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter SYNTHESIS_FSM_ENCODING "onehot,safe"Synthesis attribute for the state machine register will be generated at the output Verilog code, as follows.
reg [`W-1:0] cur_state /* synthesis syn_encoding="onehot,safe" */;
3.6.2.4.25 SYNTHESIS_ENABLE_TMR
(Ask a Question)This constraint is used to direct synthesis tools to use triple-modular redundancy (TMR) technique in the register implementation.
When this option is enabled, Synopsys attribute /* synthesis syn_radhardlevel="tmr" */ will be applied globally to the compiled design.
- Category
- HLS Constraints
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 0: disabled
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter SYNTHESIS_ENABLE_TMR 1
3.6.2.4.26 SYNTHESIS_FORCE_LOGIC_MULT
(Ask a Question)This constraint is used to force all multipliers in the compiled design to be implemented as logic, to avoid any multiplier occupies dedicated hardware DSP block resource.
When this option is enabled, Synopsys attribute /* synthesis syn_multstyle="logic" */ will be applied globally to the compiled design.
- Category
- HLS Constraints
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 0: disabled
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter SYNTHESIS_FORCE_LOGIC_MULT 1
3.6.2.4.27 ADD_SYNTHESIS_GLOBAL_ATTRIBUTE
(Ask a Question)This command allows users add any Synopsys global attribute setting to the compiled design.
- Category
- HLS Constraints
- Value Type
- String
- Valid Values
- Any legal Synopsys global attribute setting string in Verilog format
- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
add_synthesis_global_attribute {syn_hier="fixed"}Attribute
/* synthesis syn_hier="fixed" */will be generated and applied globally to the compiled design.
3.6.2.4.28 MINIMIZE_MATH_BLOCKS
(Ask a Question)This constraint is used to enable optimizations targeting the reduction of math blocks usage. It mainly affects 2 optimizations: wide-multiplication split algorithm, and multiplication by constant strength reduction. By setting this constraint to 1, SmartHLS will try to minimize the number of math blocks which can increase the latency and/or the logic elements (LUTs, DFFs) usage.
- Category
- HLS Constraint
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Values
- 0: disabled
- Location Where Default is Specified
examples/shls.tcl- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter MINIMIZE_MATH_BLOCKS 1
3.6.2.4.29 READONLY_RAM_TO_ROM
(Ask a Question)When READONLY_RAM_TO_ROM is set to 1, SmartHLS™ would analyze memory access patterns and generate read-only RAM as ROM (Read Only Memory). This constraint is enabled by default.
- Category
- HLS constraint
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 1
- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter READONLY_RAM_TO_ROM 0
3.6.2.4.30 ECC_ERROR_PROBABILITY
(Ask a Question)This constraint is used for Error Correction Code error emulation. It represents the error probability (single or double-bit errors) in software and simulation.
- Category
- HLS constraint
- Value Type
- Decimal or integer
- Valid Values
- Decimal or integer between 0.0 and 1.0 inclusive
- Default Value
- 0
- Dependencies
- None
- Applicable Flows
- RTG4™ and PolarFire® devices
- Test Status
- Actively in-use
- Examples
set_parameter ECC_ERROR_PROBABILITY 1.0
3.6.2.4.31 ECC_CORRECTION_PROBABILITY
(Ask a Question)This constraint is used for Error Correction Code error emulation. It represents the probability of a single-bit error when an error is detected in software and simulation.
- Category
- HLS constraint
- Value Type
- Decimal or integer
- Valid Values
- Decimal or integer between 0.0 and 1.0 inclusive
- Default Value
- 0
- Dependencies
- None
- Applicable Flows
- RTG4™ and PolarFire® devices
- Test Status
- Actively in-use
- Examples
set_parameter ECC_CORRECTION_PROBABILITY 0.5
3.6.2.4.32 ECC_WARNING_MSGS_ON
(Ask a Question)This constraint is used for Error Correction Code error emulation. It enable messages from the memory RTL model when an error is detected.
- Category
- HLS constraint
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 0
- Dependencies
- None
- Applicable Flows
- RTG4™ and PolarFire® devices
- Test Status
- Actively in-use
- Examples
set_parameter ECC_WARNING_MSGS_ON 1
3.6.2.4.33 ECC_ERROR_INJECTION_ON
(Ask a Question)- Category
- HLS constraint
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 0
- Dependencies
- None
- Applicable Flows
- RTG4™
- Test Status
- Actively in-use
- Examples
set_parameter ECC_ERROR_INJECTION_ON 1
3.6.2.4.34 ACTIVE_LOW_RESET
(Ask a Question)This constraint is used for enable active low reset for the generated RTL modules. Default is 0 (active high reset).
- Category
- HLS constraint
- Value Type
- Boolean
- Valid Values
- 0, 1
- Default Value
- 0
- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter ACTIVE_LOW_RESET 1