Adding a Port
(Ask a Question)To add a port to the view, right click a port in the Design Tree and select Load Selection. Adding a port to the view is the same as adding a net connected to the port.
To add a port to the view, right click a port in the Design Tree and select Load Selection. Adding a port to the view is the same as adding a net connected to the port.
Rev: 2026.1