20.1.2.5.1 QoS AXI Initiator
(Ask a Question)The QoS feature allows bandwidth to be shared among the fabric initiators while accessing DDR. To share bandwidth, an AXI initiator (referred as the QoS initiator) is connected internally at the AXI switch that performs the DDR access. This AXI initiator, which is hidden from the user, performs DDR access controlled through QoS AXI initiator parameters. The QoS is enabled only when DDR is enabled.
You can change the QoS parameter values using vsim commands while launching the
simulation. To do so, see the following table.
| Parameter | Description | Default Value |
|---|---|---|
| QOS_AXI_CLKS | Number of AXI clocks at which QoS initiator performs read/write AXI
transactions with DDR. To change the value of this parameter, use the following
| 5000 |
| QOS_START_ADDRESS | Base address for QoS operation. Change this address if the same address region is being used
by another application through FIC. To avoid contention between QoS and FIC accessing
the same DDR region, shift the QoS access region to an unused address region. To
change the value of this parameter, use the following vsim
command:For 38-bit: For 32-bit: (also
need to change DDR_ADDRESS_REGION for 32-bit) | 38'h00_C000_0000 |
| NO_OF_QOS_TRANSACTIONS | Number of burst read/write transactions performed by QoS at regular or cyclic intervals of
QOS_AXI_CLKS. If set to zero, QoS does not perform any AXI transactions
to DDR and the entire bandwidth is allocated to FICs. Note: Make sure the QOS_AXI_CLKS value is
greater than the finish time of all QoS AXI transactions. The smallest burst size
typically uses:
To change the value of this parameter, use the following
| 128 when DDR is used. |
The following shows an example of a simulation log where a fabric QoS initiator accesses DDR with number of QoS transactions set to ONE.
#
# QoS Write Transactions 1 Completed
# QoS Read Transactions 1 Completed
# Writing to DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000000, data = 12345678
# Writing to DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000001, data = aabbccdd
# Writing to DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000002, data = 12355577
# Writing to DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000003, data = aabbccdd
# Writing to DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000004, data = 12365476
# Writing to DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000005, data = aabbccdd
# Writing to DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000006, data = 12375375
# Writing to DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000007, data = aabbccdd
# Reading from DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000000, data = 12345678
# Reading from DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000001, data = aabbccdd
# Reading from DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000002, data = 12355577
# Reading from DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000003, data = aabbccdd
# Reading from DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000004, data = 12365476
# Reading from DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000005, data = aabbccdd
# Reading from DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000006, data = 12375375
# Reading from DDR3 Memory @ rank = 0, bank = 00, row = 00000, col = 00000007, data = aabbccdd