20.2.3 Creating a Project and Configuring MSS

To create a project and configure MSS:

  1. Launch the PolarFire SoC MSS Configurator (pfsoc_mss) using one of the following ways:
    • Libero SoC installation directory
    • Standalone MSS installation area
    • Windows Start menu
  2. Create a new project using Project > New. The New Project dialog is displayed.
    Figure 20-54. MSS — Module Name Dialog Box
  3. Enter a module name (for example, PFSOC_MSS_C0), and then select the appropriate die, package, and speed. The module name you enter appears in the following places:
    • File names of the PolarFire SoC MSS Configurator generated outputs at the specified output/generation directory
    • MSS component file (<module_name>.cxz)
    • MSS XML configuration file (<module_name>_mss_cfg.xml)
    • MSS configuration file corresponding to the current MSS configuration that is generated (<module_name>.cfg)
    • MSS configuration report file (<module_name>_Report.html)
    • Component/module name of the MSS component (cxz) that can be imported to a Libero SoC project
  4. The Export HDL (Netlist) option controls whether the HDL output is generated for the MSS. When enabled, the HDL representation of the MSS, that includes timing shell information, is generated and placed in the project’s output/generation directory along with other generated artifacts. This option is cleared by default.
    In Batch mode, this option can be used as follows:
     -EXPORT_HDL true | false
  5. The Use Board Preset option enables you start a new MSS project using a predefined configuration (.cfg preset) that matches a specific evaluation board or known hardware platform. Currently, the following Icicle Kit presets are available for selection.
    • Bare Metal
    • Quad Core Linux

    Presets for Icicle Kit

    When you create a New Project, you can import one of the available presets for Icicle kit. These presets are staged in data folder and are in ‘CFG’ format. All the parameter/values from the CFG file are loaded, except for the following four parameters:
    • Module Name
    • Die
    • Package
    • Speed

    User-selected values are used for Module Name, Die, Package, and Speed parameters in the GUI. This is done to facilitate changing Module Name/Die/Package/Speed (from the Icicle kit preset) to meet users need.

    The default speed grade is STD including for the Icicle Kits. If you open a previous release .cfg, which does not have speed grade (PolarFire SoC MSS Configurator v2021.2 or earlier) in v2021.3, it has STD as the default speed grade.

    The list of presets are shown using a tree widget. By default, the ‘Default Configuration’ preset is selected in GUI and user must explicitly select one of the presets for Icicle kit to load them. Once a preset is selected, users cannot edit them using Edit Settings option as the preset tree widget is unavailable in the Edit Settings dialog box.

    The following figure shows the MSS configurator tabs.

    Figure 20-55. MSS Configurator Tabs
  6. Configure Clocks, Fabric Interface Controllers, I/O Configuration, DDR Memory, and Misc settings.
  7. Click the Save option to save the MSS configuration to a .cfg file.
  8. From the Save MSS Configuration dialog box:
    • Browse to a directory and create a folder. For example, create C:\Microsemi\PFSOC_MSS_Configuration.
    • Enter a file name (for example, PFSOC_MSS_C0) and click Save.
      Note: The file name you enter is for the stand-alone MSS project only and is not used as the component name.

The MSS Configuration is created and saved to the file specified and the Log window shows the following message: INFO: Successfully saved MSS configuration in C:/Microsemi/PFSOC_MSS_Configuration/PFSOC_MSS_C0.cfg file.